Skip to main content
MKono.1
Visitor II
Jun 16, 2020 11:10 AM UTC
Solved

We are using STM32F429VET in our design. Please tell me if the internal structure of I/O port of STM32F429VET is the same.

Currently, we are testing whether smoke and fire will occur when adjacent I/O ports are shorted. If the internal structure is the same, we think that a representative set of tests is sufficient. However, if the internal structure is different, then all I/O ports must be tested.

Is the I/O port of the STM32F429VET the same from this point of view?

This topic has been closed for replies.
TDK
TDKBest answer
Jun 16, 2020 12:55 PM UTC

Most GPIO pins are the same, but there are some differences. PC13-15 and PH0-1. But unless you're shorting 3V3 to GND, nothing bad should happen. And even then, the chip will likely just reset and start working again when the short is removed.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

Uwe Bonnes
Chief
Jun 16, 2020 11:22 AM UTC

The datasheet explains the different IO Structures. Read carefully!

TDK
TDKBest answer
Jun 16, 2020 12:55 PM UTC

Most GPIO pins are the same, but there are some differences. PC13-15 and PH0-1. But unless you're shorting 3V3 to GND, nothing bad should happen. And even then, the chip will likely just reset and start working again when the short is removed.

"If you feel a post has answered your question, please click ""Accept as Solution""."