Skip to main content
arunease
Associate III
April 1, 2016
Question

watchdog

  • April 1, 2016
  • 1 reply
  • 586 views
Posted on April 01, 2016 at 11:51

Hi

i have implemented watchdog on f429. i have two applications on flash , one is  bootloader and other one is an application program . i have implemented the watchdog on bootloader and also jump function from bootloader to appllication.

My goal is to start the watchdog on bootloader, jump to application proǵram and , top the watchdog once the application gets started and runs properly.

the problem is i cant able to stop the watchdog when the application starts.

could anyone help me or suggest me some idea ?

thank you
    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    April 1, 2016
    Posted on April 01, 2016 at 12:21

    Hello,

    I think you have the same problem as this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/IWDG%20disbale%20steps%20for%20STM32F2xxSTM32F4xx&FolderCTID&currentviews=29]discussion

    According to the reference manual:

    ''Independent watchdog (IWDG): the IWDG is started by writing to its Key register or by hardware option. Once started it cannot be stopped except by a Reset.''

    I hope this can help you.

    -ForumSTM32-