Skip to main content
ezrab
Associate III
October 20, 2010
Question

watch Dog question

  • October 20, 2010
  • 4 replies
  • 824 views
Posted on October 20, 2010 at 11:29

hi

i saw that the slower watch dog i can make will reset after

 /* On Value line devices, Enable WWDG and set counter value to 127, WWDG timeout = ~1366 ×–s * 64 = 87.42 ms */

can i make it slower like 500msec?

thanks.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    October 20, 2010
    Posted on October 20, 2010 at 18:18

    Use the Independent watchdog (IWDG) it has a 12-bit counter, and an 8-bit prescaler off the 40 KHz LSI. Max timeout is in the order of 26 seconds.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ezrab
    ezrabAuthor
    Associate III
    October 21, 2010
    Posted on October 21, 2010 at 08:24

    hi.

    i tried using the IWDG but for some reason it does not work when ever it needs to reset the CSTACK gets full and it does not start.

    why?

    #include ''stm32F10x.h''

    #define IWDG_WriteAccess_Enable     ((uint16_t)0x5555)

    #define IWDG_Prescaler_32           ((uint8_t)0x03)

    #define KR_KEY_Reload    ((uint16_t)0xAAAA)

    #define KR_KEY_Enable    ((uint16_t)0xCCCC)

    #define CSR_RMVF_Set              ((uint32_t)0x01000000)

    void setsystemclock(void);

    void uartfunction(void);

    uint8_t TxBuffer[] = ''Buffer Send from USART3 to USARTz using Flags'';

    uint8_t TxCounter = 0, RxCounter = 0;

    int main(void)

    {

    char byte_temp=0;

        setsystemclock(); //set system clock to 24Mhz

        RCC->CSR |= CSR_RMVF_Set;

        //watchdog configuration

        IWDG->KR=IWDG_WriteAccess_Enable;//unlock WDG registers

        /* IWDG counter clock: 40KHz(LSI) / 32 = 1.25 KHz */

        IWDG->PR =IWDG_Prescaler_32;

        IWDG->RLR =349;//reload value

       IWDG->KR =KR_KEY_Reload;

        //IWDG->KR = KR_KEY_Enable;

        RCC->APB2ENR =RCC_APB2RSTR_IOPCRST | RCC_APB2RSTR_AFIORST;//port C clock and alternative clock enable. page 79

        RCC->APB1ENR =RCC_APB1ENR_USART3EN ;

          GPIOC->CRH=GPIO_CRH_MODE10 | GPIO_CRH_CNF10_1 |  GPIO_CRH_CNF11_0 ;//PC11 in input floating mode for RX. PC10 Alternative Output TX.

    AFIO->MAPR=AFIO_MAPR_USART3_REMAP_0 ;//port remap as uart //PC10 TX PC11 RX

        USART3->CR1 =USART_CR1_RE | USART_CR1_TE; //Receiver enable, Transmitter enable, USART disable

        USART3->BRR=0x9C4;//9600 at 24Mhz

        USART3->CR1 |= USART_CR1_UE;; //Uart Enable;

    while (((USART3->SR) & USART_SR_TXE)==0);

       USART3->DR = 'S';

    IWDG->KR = KR_KEY_Enable;

      while(1)

      {

        IWDG->KR =KR_KEY_Reload;

       if (((USART3->SR)&USART_SR_RXNE)>0)

        {

        byte_temp= USART3->DR;

         if (((USART3->SR)&USART_SR_TXE)>0)

         {

           USART3->DR =(byte_temp+1);

           while(1);//reset here

         }

        }

     /*   while(TxCounter < 30)

      {

         USART3->DR =('5');

          while(((USART3->SR)&USART_SR_TXE)==0);// Loop until USARTy DR register is empty

          TxCounter++;

      }

      TxCounter=0;*/

      }

    }

    void setsystemclock(void)

    {

          RCC->CR |= RCC_CR_HSEON;

        // Wait until it's ready

        while ((RCC->CR & RCC_CR_HSERDY) == 0)

            ;

        // Select PREDIV1 as PLL source and sett PLL mul to 3 (set bit 0)

        // for 8*3 = 24 MHz

        RCC->CFGR |= RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL_0;

        // Start PLL

        RCC->CR |= RCC_CR_PLLON;

        // Wait until it's ready

        while ((RCC->CR & RCC_CR_PLLRDY) == 0)

            ;

        // Select PLL as system clock

        RCC->CFGR |= RCC_CFGR_SW_PLL;

        // Here we can check if PLL is used, and maybe disable HSI

        // Disable HSI

        RCC->CR &= ~RCC_CR_HSION;

        RCC->CFGR|=RCC_CFGR_MCO_2; //sys clock output

    }

    ezrab
    ezrabAuthor
    Associate III
    October 21, 2010
    Posted on October 21, 2010 at 09:00

    never mind it works i tried it on adiffrent board and it works.

    i dont know what can be wrong with the older board but there is always stack full there.

    tried to erase the flash didnt help.

    mybe its becuse i removed the SB16?

    ezrab
    ezrabAuthor
    Associate III
    October 21, 2010
    Posted on October 21, 2010 at 09:53

    i checked and it is realy becuse SB16 was missing now the older board works to.

    i wonder why SB16 effects like that?