Wake up Pin from standby mode
I am using wake up PIN1 (PA0) to wake the STM32F746 from standby mode. I have PA0 connected to a push button with a pull down resistor. When first powered up the MCU goes into standby mode and stays in it until I press the button connected to PA0. The MCU wakes up for about 10 seconds and then goes into standby mode again. But then it wakes up with out me pressing the button and continues this cycle. The PA0 pin is configured as a wakeup pin.
Here is the code to detect if the MCU is woken from standby mode:
// check standby mode flag
// reset if it is still set
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear the SB flag
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1); // disable wakeup pin1
}Here is the code for putting MCU into standby mode:
void enter_standby(void){
// clear the wake up flag
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
// display Stdby Mode on the OLED
ssd1306_Fill(Black); // clear the SSD1306 OLED display
ssd1306_SetCursor(0, 0);
ssd1306_WriteString("Stdby Mode ", Font_11x18, White);
ssd1306_UpdateScreen();
/* Enable WKUP pin */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
/* Enter Standby Mode , wake up with a rising edge on PA0 */
HAL_PWR_EnterSTANDBYMode();
}Any one have any ideas why it is doing this?