Skip to main content
Associate III
Aug 28, 2025 6:23 AM UTC
Question

Wake Up from stop mode using USART (HSI for USART Clock,System clock use MSI)

Hi, 

I'm using STM32L0 MCU, My system uses MSI as the main system clock, but my USART is to use HSI to be able to wake up from stop mode. My system will enter stop mode for power saving. I am confused about the settings, before enter stop mode, we have to set system clock after STOP mode using HAL API:

__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI); // Set system clock as MSI after stop

__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI); // Set system clock as HSI after stop so that USART able to wake up the MCU

 

void PreSleepProcessing(uint32_t *ulExpectedIdleTime) {
	*ulExpectedIdleTime = 0; // WFI is called within next function
#ifdef TEST_LP_MODE
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, 0);
#endif
	if (g_diableStopModeFlags == 0) {
		while(__HAL_UART_GET_FLAG(&huart1, USART_ISR_BUSY) == SET); // Make sure that no UART transfer is on-going
		while(__HAL_UART_GET_FLAG(&huart1, USART_ISR_REACK) == RESET); // Make sure that UART is ready to receive
		HAL_UARTEx_EnableStopMode(&huart1);
		// LL_RCC_SetClkAfterWakeFromStop(RCC_STOP_WAKEUPCLOCK_MSI);
		// HAL sets STOP wakeup clock for peripherals (so UART on HSI can wake)
		__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);
		HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
	} 
}

 

Any idea how can I maintain the system clock as MSI after stop mode at the same time USART able to wake up the system from stop mode using HSI?

This topic has been closed for replies.

2 replies

ST Employee
Sep 1, 2025 8:52 AM UTC

Hello @chai2145, 

The key point is the STOPWUCK bit. The RM states:

"MSI or HSI16 RC oscillator are selected as system clock for Stop mode exit by configuring the STOPWUCK bit in the RCC_CFGR register" 

SarraS_0-1756716710846.png

Hope that helps!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
chai2145Author
Associate III
Sep 8, 2025 2:55 AM UTC
  • Before STOP: System clock using MSI. Nothing changes yet.

  • Enter STOP → system goes into low-power mode. Configured STOPWUCK bit to use HSI 

  • Exit STOP → system will switch to HSI as the system clock. 

After STOP exit, the system clock will change to HSI  instead of maintaining MSI as system clock source?