Skip to main content
bruzzim
Associate III
February 26, 2010
Question

wake up from stop mode on usart interrupt: do I need to configure EXTI?

Posted on February 26, 2010 at 12:31

wake up from stop mode on usart interrupt: do I need to configure EXTI?

    This topic has been closed for replies.

    4 replies

    Tomas DRESLER
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    In STOP mode USART clock is off, too. To detect incoming packet, you have to use EXTI wake-up as this is the only suitable peripheral able to wake your MCU up.

    Next, you have to consider that STM32 will wake up on 8 MHz clock and it will take few ms to switch on HSE and PLL again => the first byte may be wrong and your protocol has to count with that.
    bruzzim
    bruzzimAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Thanks again, edison.

    Barbie
    Associate III
    May 4, 2013
    Posted on May 04, 2013 at 09:31

    So if I get it right. The UART frame itself can't wake up the MCU from stop mode. I need to make same kind of HW line taht give me pulse on GPIO when I receive UART frame. Is it so?

    Bar.

    Tesla DeLorean
    Guru
    May 4, 2013
    Posted on May 04, 2013 at 16:33

    You're bigger problem is that it will miss the first byte, at least.

    I seem to recall one of the F0/F3 seminars of a low power mode where the function of the USART was maintained.

    The alternative would be a method using a RTS/CTS based handshake to wake up the part first, and then indicate it could receive new data.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..