Skip to main content
JAlca
Associate III
March 11, 2021
Question

Wake up from stand by from a tamper pin.

  • March 11, 2021
  • 4 replies
  • 1647 views

Hi all,

It is possible to wake up a STM32F3 series MCU, in stand by mode, from a tamper pin?

This topic has been closed for replies.

4 replies

Uwe Bonnes
Chief
March 11, 2021

RM0316. chapter 7.3.5:

Mode exit:

         WKUP pin rising edge, RTC alarm event's rising edge, external Reset in

         NRST pin, IWDG Reset.

I/O states in Standby mode

In Standby mode, all I/O pins are high impedance except:

·   Reset pad (still available)

·   TAMPER pin if configured for tamper or calibration out

·   WKUP pin, if enabled

JAlca
JAlcaAuthor
Associate III
March 11, 2021

Yes, but in the same chapter, it says:

--------------------------------------------------------------------

Standby mode Description

Mode entry

WFI (Wait for Interrupt) or WFE (Wait for Event) while:

– Set SLEEPDEEP in ARM® Cortex®-M4 System Control register

– Set PDDS bit in Power Control register (PWR_CR)

– Clear WUF bit in Power Control/Status register (PWR_CSR)

Mode exit WKUP pin rising edge, RTC alarm event’s rising edge, external Reset in

NRST pin, IWDG Reset.

--------------------------------------------------------------------

It dont talk about tamper pins, only wakeup pins.

Uwe Bonnes
Chief
March 11, 2021

So use wakeup pin as tamper.

JAlca
JAlcaAuthor
Associate III
March 11, 2021

I did it, and its work well. But the wakeup pin is only rising edge active, and I need a falling edge (yes, I can use a NOT gate, but if is there a way to use tamper...)