Skip to main content
Associate III
Jul 3, 2024 8:21 AM UTC
Question

Vss pin setting

Hi.

 

I'm using STM32F303RCT6 now.

 

Is it possible to set one pin vss using gpio settings?

If so, is there a specific pin?

 

If you have any question, ask me.

Thank you. 

This topic has been closed for replies.

6 replies

mƎALLEm
ST Technical Moderator
Jul 3, 2024 8:23 AM UTC

Hello,

Not sure what do you mean by this:


Is it possible to set one pin vss using gpio settings?

If so, is there a specific pin?


Could you please clarify?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
giwonKIMAuthor
Associate III
Jul 3, 2024 11:43 PM UTC

There are 4 Vss pins in MCU : STM32F303RCT6.

 

I want to add 1 Vss pin in there.

 

How can i add it?

 

Is it impossible?

Karl Yamashita
Super User
Jul 4, 2024 1:09 AM UTC

@giwonKIM wrote:

There are 4 Vss pins in MCU : STM32F303RCT6.

 

I want to add 1 Vss pin in there.

 

How can i add it?

 

Is it impossible?


You're still not very clear on what you're trying to achieve?

You want to add 1 Vss pin to among the already 4 Vss pins to make 5 Vss pins? Or are you wanting to convert 1 of Vss pin to a GPIO?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
giwonKIMAuthor
Associate III
Jul 4, 2024 1:19 AM UTC

Hi.

 

I'm trying to add 1 Vss pin to make 5 Vss pins.

 

 

Karl Yamashita
Super User
Jul 4, 2024 1:27 AM UTC

And this extra Vss pin is supposed to do what?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source