Question
Virtual COM Port on STM32L053 w/IDB04A1 ?
Posted on December 24, 2014 at 19:03
According to the documentation and the release notes, it looks like I should be able to either download the binary or a rebuilt HEX file for the VirtualCOMPort project to the STM32L053 Nucleo board and then connect this board to a PC via the USB port and the BlueNRG GUI on the PC ought to be able to communicate with the BlueNRG IC.
Yet, when I load this project onto the hardware and then connect the board to the PC there is no COM port. I even installed the COM port driver from the BlueNRG GUI package.Is there something else we need to do to make this combination work?