Question
Virtual Com Port Loopback runs w/o debugger not w/ debugger
Posted on September 26, 2013 at 18:01
Greetings,
I've brought up the ST example VirtualComPort_Loopback (V4.0.0) on a Keil demo board (MCBSTM32E vers3) and the Keil enviroment (uVision 4.71.2.0) connecting through the ST virtual comport driver (1.3.1.0) and it works fine when not run from within the debugger. When run from within the debugger, however, the terminal emulator (PuTTY) error's out with: ''Unable to open connection to Com46, Unable to configure serial port''. The Com port (46) does show up in device manager and no errors are indicated.My uneducated guess is that the ST virtual comport driver is not happy something that's different in it's interaction over the USB connection when the debugger is running and it's refusing the terminal emulators connection.I would really appreciate any ideas for chasing this problem down as the problem also exists on a custom board with a complex application in need of enhancing and debugging...Thanks in advance.Steve.