Skip to main content
dschneeweis
Associate II
May 12, 2008
Question

Verify with anglia

Posted on May 12, 2008 at 06:38

Verify with anglia

    This topic has been closed for replies.

    6 replies

    dschneeweis
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    Hello

    I am not sure if this is the right forum for my question.

    I am using the anglia idealist with the sarm tool-chain. I implemented an addtional section in the linkerscript. Everything works fine. Only the verification after programming the flash fails if i use the additional section. If i just use the standart section verifing is ok.

    Is it possible to tell the verification tool, that there is a new section?

    sjo
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    Hi,

    What version of the toolchain/ide are you using?

    Try programming using a different format, eg. binary. and see whether that passes verify.

    Cheers

    sjo

    dschneeweis
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    ???

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    Hi sjo

    I believe that this is for you :)

    Cheers,

    STOne-32.

    sjo
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    Post the linker script here, and i will look into it

    Cheers

    sjo

    dschneeweis
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    Hi

    I am using Angle IDEalist 1.61.

    If I change to one of the other formats, e.g. Motorola s19, verifing fails too and debugging with these formats doesn't work.