Vector table relocation works only in debug mode
Hi,
I'm facing a problem with relocation of the vector table to the internal SRAM. I work with the STM32F030CCT6 (using the Ac6 System Workbench and CubeMX, with the HAL libraries 1.9.0) and I want to design a simple bootloader.
This is a part of my linker script:
/* Specify the memory areas */
MEMORY{RAM (xrw) : ORIGIN = 0x200000C0, LENGTH = 32K-0xC0VTRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 0xC0FLASH (rx) : ORIGIN = 0x08000800, LENGTH = 256K-0x800}....RAMVectorTable(NOLOAD): {*(.RAMVectorTable)} >VTRAMThis is a vector table relocation in the main() of the bootloader:
__IO uint32_t VectorTable[48] __attribute__((section('.RAMVectorTable')));
/* USER CODE END 0 *//** * @brief The application entry point. * * @retval None */int main(void){ /* USER CODE BEGIN 1 */ uint32_t i = 0; for(i = 0; i < 48; i++) VectorTable[i] = *(__IO uint32_t*)((uint32_t)0x08000800 + (i<<2)); /* Enable the SYSCFG peripheral clock*/ __HAL_RCC_SYSCFG_CLK_ENABLE(); /* Remap SRAM at 0x00000000 */ __HAL_SYSCFG_REMAPMEMORY_SRAM();...Later on I send some test messages over the UART interface. I do not know why, but the above code works perfectly in the debug mode - I just need to run 'debug' and then 'resume' the program execution (with or without breakpoints later, does not matter).
Nevertheless, if I program the target (right click on the project -> 'Target' -> 'Program chip...', or just power-reset what I uploaded during the debug session), there is no response from the board. I am pretty sure that finally there is the same program on flash since I use the same .elf file both for the debugging session and regular programming... However, I've checked that if I do not relocate the vector table and I program the flash from the beginning (flash starts at 0x08000000), everything works just fine.
Just to clarify - I want to program the bootloader with some offset (0x0800) in memory because I need some space for the bootloader sensitive data (bootheader).
BR,
Marek