Skip to main content
anoop
Associate II
June 1, 2012
Question

VCP example

Posted on June 01, 2012 at 12:17

Can anyone post a link to a working Virtual COM port example for the STM32F4 discovery board.

-gandalf

#vcp-download-drivers
    This topic has been closed for replies.

    14 replies

    jlchoobs
    Associate III
    June 2, 2012
    Posted on June 02, 2012 at 19:09

    Gandalf,

    See my project :

    New Project Download - Virtual Com with Cmd Shell and ADC Reading

    Page - see Virtual Com Project for Descriptrion and Download :

    [[this link/image has been flagged as malicious by our security scan software and has been deleted]]

    https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New%20Project%20Download%20-%20Virtual%20Com%20with%20Cmd%20Shell%20and%20ADC%20Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=318

    anoop
    anoopAuthor
    Associate II
    June 4, 2012
    Posted on June 04, 2012 at 11:34

    Thanks for the quick reply jlc.jlsilicon. I code is running fine. Could you please provide me with a link to the serial.inf driver, i am using windows xp SP3. If would really appreciate it if you could give me a link from where i can download the driver.

    -Gandalf

    anoop
    anoopAuthor
    Associate II
    June 4, 2012
    Posted on June 04, 2012 at 20:26

    jlsilicon,

               Ive installed the VCP driver that STmicro provides in its website. With the code running on the board when connected to the PC, XP asks me to install a driver for the USB device. Which driver do i install ? I little help would be appreciated.

    -gandalf

    jlchoobs
    Associate III
    June 5, 2012
    Posted on June 05, 2012 at 10:40

    Okay Gandalf,

    Let me see if I can find it, or modify the code with an alternate.

    kelnerrr
    Visitor II
    July 24, 2012
    Posted on July 24, 2012 at 21:14

    Hello,

    I also have a problem with finding working virtual COM port drivers for this project. Anyone could provide a link, please? I am running Windows 7 64-bit.

    Thanks,

    Kelnerrr

    Tesla DeLorean
    Guru
    July 24, 2012
    Posted on July 24, 2012 at 21:42

    Page - see Virtual Com Project for Descriptrion and Download :

     

    Wikisend links are broken.

    https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=318

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    kelnerrr
    Visitor II
    July 24, 2012
    Posted on July 24, 2012 at 22:08

    Hi Clive,

    I've searched the project page for any info where to grab the working driver for vcp. No luck. Would you mind sending it to kelnerrr at gmail.com?

    Thanks,

    Kelnerrr

    Tesla DeLorean
    Guru
    July 24, 2012
    Posted on July 25, 2012 at 00:48

    I've emailed you, but for general consumption these are the most recent VCP drivers I'm aware of.

    http://dekar.wc3edit.net/st website/VCP_Setup.zip

    http://www.st.com/stonline/stappl/resourceSelector/app?page=resourceSelector&doctype=SW_DRIVER&ClassID=1734

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/stm32_vcp.zip

    https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=318

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    July 25, 2012
    Posted on July 25, 2012 at 23:33

    Going to confirm from my own testing that the last link, which contains the v1.3.1 drivers for x64 works in Win 7 against a VCP/CDC example built from the USB FW library which I have ported.

    STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\VCP

    https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=318

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    aljaz
    Visitor II
    April 3, 2013
    Posted on April 03, 2013 at 10:11

    Hello,

    it looks like ST has made major changes on the website and removed all the USB firmware and VCP drivers. Only 3rd party firware is left available.

    Does anybody have the latest VCP drivers?

    Thanks!