Skip to main content
rumlyen
Associate III
September 16, 2016
Question

VCP driver issue for Windows 7. can recognize in Windows 10

  • September 16, 2016
  • 1 reply
  • 462 views
Posted on September 16, 2016 at 23:29

Hello all.

Windows 10 can well recognize my STM32L1 device (custom PCB) as 'USB Serial device' but same isn't recognizing in Windows 7 (another PC). I've tried both VCP driver 1.3 and 1.4 in windows 7. Do I need to change any configuration anywhere to make it run in Windows 7. I've used USB_FS_4.0 library in this project.

I appreciate your comments here.
    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    September 29, 2016
    Posted on September 29, 2016 at 16:24

    Hello,

    Do you get an error message ?

    If you can test and check this issue with another Pc (Windows 7), in order to deduce if the problem here seems related to the hardware or software environment.

    Regards