Skip to main content
MikeDB
Senior II
Feb 18, 2019 11:01 PM UTC
Solved

VCAP layout

I'm sure everyone else has noticed how the two pins to VCAP seem to be placed just over a complete side of the package away so there is bound to be some resistance/inductance in the tracking. I was wondering if anybody has ever hit problems with this, or how thick the tracking should be. Also the datasheets and app notes seem a bit inconsistent, some say 2.2uF, some two 2.2uF in parallel and others 4.7uF. Prefer to get the board right first time. Processor is a STMH7 series in 100 pin QFP

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Feb 19, 2019 10:25 PM UTC

You are not supposed to connect those two VCAP pins with a track, and you are supposed to place a 2.2uF cap on each.

Get inspired with the Nucleo, I know it's a 144-pin package but the principle is the same.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
Feb 19, 2019 10:25 PM UTC

You are not supposed to connect those two VCAP pins with a track, and you are supposed to place a 2.2uF cap on each.

Get inspired with the Nucleo, I know it's a 144-pin package but the principle is the same.

JW

MikeDB
MikeDBAuthor
Senior II
Feb 19, 2019 10:32 PM UTC

Ah that makes more sense. Thanks