Associate
December 15, 2021
Question
Vbat pin drawn high currebt when power is off
- December 15, 2021
- 14 replies
- 5066 views
I am using Nucleo 144 H745ZQi , connected vbat pin directly using coin cell, when power is off/unconnected, LD7 led ovcr indicator turned on and current consumption drawn from baterry was 50mA, also the LD5 led turned on. However when i reconnect the power, either using option jumper on stlink or ext 5V then the LD7 turn off and it seems normal again. I wonder why? Please help me, because it's will waste the battery when used power off.