Skip to main content
Marcel Blindu
Associate III
Jan 16, 2019 9:12 AM UTC
Question

Values Capacitor HSE & LSE

Which values can I suppose for Cin, Cout and Board Strays for STM32F103 and STM32L4 for HSE and LSE using the ecuation 1 in the following datasheet of the abracon "https://abracon.com/uploads/resources/PierceOscillator_Fundamentals.pdf"

    This topic has been closed for replies.

    6 replies

    Uwe Bonnes
    Chief
    Jan 16, 2019 10:01 AM UTC

    Have a look at AN2867.

    Marcel Blindu
    Associate III
    Jan 16, 2019 10:15 AM UTC

    This values don't appear in the datasheet AN2867

    Pevy.Andy
    Associate III
    Jan 16, 2019 11:22 AM UTC

    Look at the very last line of section 3.3

    Marcel Blindu
    Associate III
    Jan 16, 2019 12:18 PM UTC

    Is the same formula for HSE and LSE for all SMT32 microcontrollers?

    CL=(CL1*CL2)/(CL1+CL2) + Cs

    and the Cs we can suppose 5pF?

    Pevy.Andy
    Associate III
    Jan 16, 2019 12:27 PM UTC

    Seems reasonable.

    Marcel Blindu
    Associate III
    Jan 25, 2019 2:54 PM UTC

    How to prove if the selection of the load capacitors CL1 and CL2 is correct?

    Maybe with oscilloscope?