Skip to main content
Associate
July 17, 2023
Question

Using TIM2 for PWM, code is getting stuck after some time.

  • July 17, 2023
  • 5 replies
  • 2979 views

Hey Everyone,
I am new to STM platform and dont have much experience with Embedded C. Currently I am stuck at PWM. 
First Things First:

I am using STM32L052C8T6 MCU with a 16MHz external Crystal Connected.
I am using STM32CubeIDE v1.12.1
I have a photodiode connected to PA3, a stepper motor driver connected to PA4-8, PA15 and an LED Driver at PA0.

The Flow of the code goes something like this:

The photodiode detects if light falling on it is more than 1000 (out of 4096 (12bit)). If so then the stepper is rotated anticlockwise and then the LED driver is given a PWM signal (100% duty cycle in this case) and then the LED is turned off and Stepper is moved back to its original position and the code loops until we get another reading above 1000.

The Problem:

The code is initially running fine. After some time the code is always getting stuck at  this line
TIM2->CCR1 = 65535;

I ran the code in debug mode without any breakpoints, when the code got stuck, NMI_Handler() function had been opened. I don't know what to make of it.

I followed the following tutorial for this https://deepbluembedded.com/stm32-pwm-example-timer-pwm-mode-tutorial/ . Please forgive me if this is a very dumb mistake.

Here is my full code for reference. 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "string.h"
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */


/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
void print(UART_HandleTypeDef *huart, char _out[]);
void println(UART_HandleTypeDef *huart, char _out[]);
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc;

I2C_HandleTypeDef hi2c1;

UART_HandleTypeDef hlpuart1;

TIM_HandleTypeDef htim2;

/* USER CODE BEGIN PV */
char text[100];
uint8_t buff[50];
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM2_Init(void);
static void MX_ADC_Init(void);
static void MX_I2C1_Init(void);
static void MX_LPUART1_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void I2C_Scan(){
	/*-[ I2C Bus Scanning ]-*/
	uint8_t ret;

	for(int i=1; i<128; i++)
	{
	 ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 3, 5);
	 if (ret != HAL_OK) /* No ACK Received At That Address */
	 {
		 sprintf(text, "No I2C Address Found\n\r");
		 HAL_UART_Transmit( &hlpuart1, (uint8_t *)text, strlen( (char*)text ), 0xFFFF );
	 }
	 else if(ret == HAL_OK)
	 {
		 sprintf(text, "I2C address is 0x%x\n\r", i);
		 HAL_UART_Transmit( &hlpuart1, (uint8_t *)text, strlen( (char*)text ), 0xFFFF );
	 }
	}
	sprintf( text,"I2C Scan Done\n\r");
	HAL_UART_Transmit( &hlpuart1, (uint8_t *)text, strlen( (char*)text ), 0xFFFF );
	/*--[ Scanning Done ]--*/
}
void Stepper_Clockwise(int angle, int speed){
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
	for(int i = 0; i<5;i++){
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
		HAL_Delay(1);
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
		HAL_Delay(1);
	}
}

void Stepper_AntiClockwise(int angle, int speed){
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
	for(int i = 0; i<5;i++)
	{
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
		HAL_Delay(1);
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
		HAL_Delay(1);
	}
}


/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 uint16_t AD_RES = 0;


 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_TIM2_Init();
 MX_ADC_Init();
 MX_I2C1_Init();
 MX_LPUART1_UART_Init();
 /* USER CODE BEGIN 2 */

 // HAL_TIM_Base_Start(&htim2);
 HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);

 // Calibrate The ADC On Power-Up For Better Accuracy
 HAL_ADCEx_Calibration_Start(&hadc, ADC_SINGLE_ENDED);

 // I2C_Scan();

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
		HAL_ADC_Start(&hadc);
		// Poll ADC1 Perihperal & TimeOut = 1mSec
		HAL_ADC_PollForConversion(&hadc, 1);
		// Read The ADC Conversion Result & Map It To PWM DutyCycle
		AD_RES = HAL_ADC_GetValue(&hadc);
		sprintf( (char*)buff, "ADC Value: %d \n\r", AD_RES);
		HAL_UART_Transmit( &hlpuart1, buff, strlen( (char*)buff ), 0xFFFF );
		if(AD_RES > 1000){
			HAL_ADC_Stop(&hadc);
			HAL_Delay(1000);
			Stepper_AntiClockwise(18, 600);
			HAL_Delay(1000);
			TIM2->CCR1 = 65535;
			HAL_Delay(1000);
			TIM2->CCR1 = 0;
			HAL_Delay(1000);
			Stepper_Clockwise(18, 600);
			HAL_Delay(1000);
		}
		HAL_Delay(100);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_I2C1;
 PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
 PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC_Init(void)
{

 /* USER CODE BEGIN ADC_Init 0 */

 /* USER CODE END ADC_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC_Init 1 */

 /* USER CODE END ADC_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc.Instance = ADC1;
 hadc.Init.OversamplingMode = DISABLE;
 hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ContinuousConvMode = DISABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.DMAContinuousRequests = DISABLE;
 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerFrequencyMode = DISABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel to be converted.
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC_Init 2 */

 /* USER CODE END ADC_Init 2 */

}

/**
 * @brief I2C1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2C1_Init(void)
{

 /* USER CODE BEGIN I2C1_Init 0 */

 /* USER CODE END I2C1_Init 0 */

 /* USER CODE BEGIN I2C1_Init 1 */

 /* USER CODE END I2C1_Init 1 */
 hi2c1.Instance = I2C1;
 hi2c1.Init.Timing = 0x00303D5B;
 hi2c1.Init.OwnAddress1 = 0;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Analogue filter
 */
 if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Digital filter
 */
 if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C1_Init 2 */

 /* USER CODE END I2C1_Init 2 */

}

/**
 * @brief LPUART1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_LPUART1_UART_Init(void)
{

 /* USER CODE BEGIN LPUART1_Init 0 */

 /* USER CODE END LPUART1_Init 0 */

 /* USER CODE BEGIN LPUART1_Init 1 */

 /* USER CODE END LPUART1_Init 1 */
 hlpuart1.Instance = LPUART1;
 hlpuart1.Init.BaudRate = 115200;
 hlpuart1.Init.WordLength = UART_WORDLENGTH_7B;
 hlpuart1.Init.StopBits = UART_STOPBITS_1;
 hlpuart1.Init.Parity = UART_PARITY_NONE;
 hlpuart1.Init.Mode = UART_MODE_TX_RX;
 hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&hlpuart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN LPUART1_Init 2 */

 /* USER CODE END LPUART1_Init 2 */

}

/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 65535;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */
 HAL_TIM_MspPostInit(&htim2);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6
 |GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_15, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0|GPIO_PIN_2, GPIO_PIN_RESET);

 /*Configure GPIO pins : PA1 PA4 PA5 PA6
 PA7 PA8 PA15 */
 GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6
 |GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PA2 */
 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PB0 PB2 */
 GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 P.S. I also intend to use an I2C sensor in this device, Hence the I2C Scan function in the code. 

This topic has been closed for replies.

5 replies

ST Employee
July 18, 2023

Dear @Anmol.jindal,

As yo mention a NMI, can we check the following points:

  • Is CSSHSEON set in RCC_CR?
  • Is CSSHSEF set when you enter in NMI?

The only way to raise a NMI in your system is caused by a HSE clock failure. So, let check first this point.

Best Regards,

Gwénolé

LCE
Principal II
July 18, 2023

First of all: very good description of your problem, including the relevant source code, and that in "style"! Doesn't happen often here.

As Gwénolé already said it is probably a clock related issue. Have you checked crystal connection and capacitors? Or can you try another clock source? Maybe just for testing try the HSI.

Anyway, what's happening if you remove the timer CCR settings and toggle another IO / LED?

And as I don't know that STM32, CPU and all peripherals running on the 16 MHz?
And what's the ADC's clock source for that STM?
If it's 16 MHz you are sampling quite fast and should use the ADC clock prescaler and / or increase its sampling time.

Associate
July 18, 2023

First of all: Thanks LCE and Gwenole for your replies.
Yes it was indeed a clock related issue. I was using HSE for the CPU and all  the peripherals and had set the Internal Clock as Clock Source for ADC (This may be the issue idk). I switched the clock source for the whole CPU as well as peripherals from HSE to PLLCLK (Clock Frequency still at 16MHz) and the code worked just fine. 
Though I am still not using any Prescaler (it is set to 0) and the Clock Period is set to 65535. With Auto Reload Turned ON. This is for anyone else venturing into this Topic anytime.

Though I would still like to know what was the issue with using an external clock. I want to know how to configure these settings and how to precisely use these Prescaler and Clock Period. So any resource(a video would be great) on how to properly use all these clock configurations would be great. Also regarding the crystal connections and capacitors, will check and update you guys.

Once again thanks guys and hoping for further updates.

LCE
Principal II
July 19, 2023

Interesting, but as I said I don't know the clock tree / routing of that STM.

Right now you are still using HSE as the source for the PLL, or HSI?

If it's HSE that's causing the trouble it might indeed be a hardware related problem, check the application notes.
Not sure it it is this one: 
https://www.st.com/resource/en/application_note/an2867-oscillator-design-guide-for-stm8afals-stm32-mcus-and-mpus-stmicroelectronics.pdf