Skip to main content
Sandhya Sharma
Associate II
Nov 2, 2017 6:43 AM UTC
Question

Using the STM32F0 ADC in DMA one shot mode and polling when the DMA is not enabled?

Posted on November 02, 2017 at 07:43

I have configured the ADC in discontinuous mode and sampling 6 channels using DMA which is configured in one shot mode. Also, I would like to poll for the ADC conversions for other channels when the DMA is not active. The DMA is enabled from a timer ISR. Is this feasible? 

    This topic has been closed for replies.