Skip to main content
T J
Senior III
September 7, 2018
Question

Using the inline compiling macro ?

  • September 7, 2018
  • 13 replies
  • 1965 views

I have an LCD is on an 8080 16bit FMC interface with A0 register select.

I can read the status correctly here:

#define LCD1_DEVICE_ADDR (uint32_t)0x60000000
#define LCD1_DEVICE_DATA (uint32_t)0x60000001
 
 uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR;
 readLcdStatus = *pLcdRStatusWAddress;
 
 

All of these snippets are within one file,

//this compiles:
 
inline lcdRegDataWrite(uint8_t reg, uint8_t data) {
 *(__IO uint16_t*)LCD1_DEVICE_ADDR = reg; 
 *(__IO uint16_t*)LCD1_DEVICE_DATA = data; 
} 
 
//but this doesn't find it
 
 lcdRegDataWrite( 1 , 8);
 
>>> undefined reference to `lcdRegDataWrite'
 
 

    This topic has been closed for replies.

    13 replies

    Amel NASRI
    ST Technical Moderator
    September 12, 2018

    Hi @Community member​ ,

    Could you please provide more details on your case: which compiler? which device? is this your own code or found in an example provided by ST?...

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    September 12, 2018

    Check with your compiler vendor, review example others are using and that work

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    T J
    T JAuthor
    Senior III
    September 13, 2018

    this is the full compiler output...

    1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
    1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln" on local computer
    1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(2):
    1>../../TH218/Lefty/lcd.c: In function 'initRa8877Pins':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(65,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
    1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
    1> ^~~~~~~~~~~~~~~~
    1>../../TH218/Lefty/lcd.c: In function 'initRA8877':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(84,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
    1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
    1> ^~~~~~~~~~~~~~~~
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(14,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_DATA (uint32_t)0x60000001
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(87,26): note : in expansion of macro 'LCD1_DEVICE_DATA'
    1> uint16_t *pLcdData = LCD1_DEVICE_DATA;
    1> ^~~~~~~~~~~~~~~~
    1>C:/SysGCC/arm-eabi/bin/arm-eabi-g++.exe -o Debug/TH218_sln.elf -Wl,-gc-sections --specs=nano.specs --specs=nosys.specs -TC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32H7xxxx/LinkerScripts/STM32H753BI_flash.lds -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wl,--start-group Debug/bios.o Debug/lcd.o Debug/sdram.o Debug/Ra8876_Lite.o Debug/usb_device.o Debug/usbd_conf.o Debug/usbd_desc.o Debug/usbd_cdc_if.o Debug/stm32h7xx_it.o Debug/stm32h7xx_hal_msp.o Debug/stm32h7xx_hal_timebase_TIM.o Debug/main.o Debug/system_stm32h7xx.o Debug/stm32h7xx_hal.o Debug/stm32h7xx_hal_adc.o Debug/stm32h7xx_hal_adc_ex.o Debug/stm32h7xx_hal_rtc.o Debug/stm32h7xx_hal_rtc_ex.o Debug/stm32h7xx_hal_fdcan.o Debug/stm32h7xx_hal_rng.o Debug/stm32h7xx_ll_fmc.o Debug/stm32h7xx_hal_nand.o Debug/stm32h7xx_hal_spi.o Debug/stm32h7xx_hal_spi_ex.o Debug/stm32h7xx_hal_mdma.o Debug/stm32h7xx_ll_sdmmc.o Debug/stm32h7xx_hal_sd.o Debug/stm32h7xx_hal_sd_ex.o Debug/stm32h7xx_hal_hsem.o Debug/stm32h7xx_hal_cortex.o Debug/stm32h7xx_hal_cryp.o Debug/stm32h7xx_hal_cryp_ex.o Debug/stm32h7xx_hal_dma.o Debug/stm32h7xx_hal_dma_ex.o Debug/stm32h7xx_hal_i2c.o Debug/stm32h7xx_hal_i2c_ex.o Debug/usbd_core.o Debug/usbd_ctlreq.o Debug/usbd_ioreq.o Debug/usbd_cdc.o Debug/stm32h7xx_hal_spdifrx.o Debug/stm32h7xx_hal_uart.o Debug/stm32h7xx_hal_uart_ex.o Debug/stm32h7xx_hal_pwr.o Debug/stm32h7xx_hal_pwr_ex.o Debug/stm32h7xx_hal_sram.o Debug/stm32h7xx_hal_flash.o Debug/stm32h7xx_hal_flash_ex.o Debug/stm32h7xx_hal_gpio.o Debug/stm32h7xx_hal_hash.o Debug/stm32h7xx_hal_hash_ex.o Debug/stm32h7xx_hal_pcd.o Debug/stm32h7xx_hal_pcd_ex.o Debug/stm32h7xx_ll_usb.o Debug/stm32h7xx_hal_hrtim.o Debug/stm32h7xx_hal_rcc.o Debug/stm32h7xx_hal_rcc_ex.o Debug/stm32h7xx_hal_crc.o Debug/stm32h7xx_hal_crc_ex.o Debug/stm32h7xx_hal_eth.o Debug/stm32h7xx_hal_tim.o Debug/stm32h7xx_hal_tim_ex.o Debug/stm32h7xx_hal_sai.o Debug/stm32h7xx_hal_sai_ex.o Debug/stm32h7xx_hal_sdram.o Debug/stm32h7xx_hal_qspi.o Debug/startup_stm32h753xx.o Debug/bsp_driver_sdram.o Debug/sdram_diskio.o Debug/fatfs.o Debug/diskio.o Debug/ff.o Debug/ff_gen_drv.o Debug/syscall.o -Wl,--end-group
    1>Debug/lcd.o: In function `initRA8877':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(95): error : undefined reference to `lcdRegDataWriten'
    1>collect2.exe : error : ld returned 1 exit status
    1>make: *** [Debug/TH218_sln.elf] Error 1
    1>-------------------------------------------------------------
    1>Command exited with code 2
    1>Executable: C:\SysGCC\arm-eabi\bin\make.exe
    1>Arguments: CONFIG=Debug -j4
    1>Directory: C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln
    1>VisualGDB : error : Command-line action failed
    1>C:\Program Files (x86)\Microsoft Visual Studio\2017\Community\Common7\IDE\VC\VCTargets\Microsoft.MakeFile.Targets(44,5): error MSB3073: The command ""C:\Program Files (x86)\Sysprogs\VisualGDB\\VisualGDB.exe" /build "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\TH218_sln.vcxproj" "/solution:C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln.sln" "/config:Debug" "/platform:Win32"" exited with code 1.
    1>Done building project "TH218_sln.vcxproj" -- FAILED.
    ========== Build: 0 succeeded, 1 failed, 0 up-to-date, 0 skipped ==========

    waclawek.jan
    Super User
    September 13, 2018

    The extra 'n' at the end of

    lcdRegDataWriten

    ?

    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(95): error : undefined reference to `lcdRegDataWriten'

    JW

    T J
    T JAuthor
    Senior III
    September 13, 2018

    Yes, I renamed it for the forum, .. well spotted..

    I added the Void but that didn't help.

    inline void lcdRegDataWriten(char reg, char data) {
    // *(__IO uint16_t*)LCD1_DEVICE_ADDR = reg; 
    // *(__IO uint16_t*)LCD1_DEVICE_DATA = data; 
     *(__IO uint16_t*)0x60000000 = reg; 
     *(__IO uint16_t*)0x60000001 = data; 
    } 

    waclawek.jan
    Super User
    September 13, 2018

    Okay so post the whole offending file which caused the output above, or post the file together with the output, so we have a complete view.

    Also, try to add a line

    #error "no compile"

    just below the line

    inline void lcdRegDataWriten(char reg, char data) {

    JW

    T J
    T JAuthor
    Senior III
    September 19, 2018

    thanks for the pointers @Community member,​ @Community member​ 

    was this the output you expected ?

    1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
    1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "VS2018\TH218_sln\TH218_sln" on local computer
    1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
    1>../../TH218/Lefty/lcd.c: In function 'lcdRegDataWriten':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(16,2): error : #error "no compile"
    1> #error "no compile"

    and this is the current code:

    inline void lcdRegDataWriten(char reg, char data) {
    #error "no compile"
    // *(__IO uint16_t*)LCD1_DEVICE_ADDR = reg; 
    // *(__IO uint16_t*)LCD1_DEVICE_DATA = data; 
     *(__IO uint16_t*)0x60000000 = reg; 
     *(__IO uint16_t*)0x60000001 = data; 
    } 

    this is the usage:

     lcdRegDataWriten(1, 8);
     
     
    with #error compile removed:
     
     
    1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
    1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln" on local computer
    1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(2):
    1>../../TH218/Lefty/lcd.c: In function 'initRa8877Pins':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(64,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
    1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
    1> ^~~~~~~~~~~~~~~~
    1>../../TH218/Lefty/lcd.c: In function 'initRA8877':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(83,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
    1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
    1> ^~~~~~~~~~~~~~~~
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(14,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
    1> #define LCD1_DEVICE_DATA (uint32_t)0x60000001
    1> ^
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(86,26): note : in expansion of macro 'LCD1_DEVICE_DATA'
    1> uint16_t *pLcdData = LCD1_DEVICE_DATA;
    1> ^~~~~~~~~~~~~~~~
    1>C:/SysGCC/arm-eabi/bin/arm-eabi-g++.exe -o Debug/TH218_sln.elf -Wl,-gc-sections --specs=nano.specs --specs=nosys.specs -TC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32H7xxxx/LinkerScripts/STM32H753BI_flash.lds -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wl,--start-group Debug/bios.o Debug/lcd.o Debug/sdram.o Debug/Ra8876_Lite.o Debug/usb_device.o Debug/usbd_conf.o Debug/usbd_desc.o Debug/usbd_cdc_if.o Debug/stm32h7xx_it.o Debug/stm32h7xx_hal_msp.o Debug/stm32h7xx_hal_timebase_TIM.o Debug/main.o Debug/system_stm32h7xx.o Debug/stm32h7xx_hal.o Debug/stm32h7xx_hal_adc.o Debug/stm32h7xx_hal_adc_ex.o Debug/stm32h7xx_hal_rtc.o Debug/stm32h7xx_hal_rtc_ex.o Debug/stm32h7xx_hal_fdcan.o Debug/stm32h7xx_hal_rng.o Debug/stm32h7xx_ll_fmc.o Debug/stm32h7xx_hal_nand.o Debug/stm32h7xx_hal_spi.o Debug/stm32h7xx_hal_spi_ex.o Debug/stm32h7xx_hal_mdma.o Debug/stm32h7xx_ll_sdmmc.o Debug/stm32h7xx_hal_sd.o Debug/stm32h7xx_hal_sd_ex.o Debug/stm32h7xx_hal_hsem.o Debug/stm32h7xx_hal_cortex.o Debug/stm32h7xx_hal_cryp.o Debug/stm32h7xx_hal_cryp_ex.o Debug/stm32h7xx_hal_dma.o Debug/stm32h7xx_hal_dma_ex.o Debug/stm32h7xx_hal_i2c.o Debug/stm32h7xx_hal_i2c_ex.o Debug/usbd_core.o Debug/usbd_ctlreq.o Debug/usbd_ioreq.o Debug/usbd_cdc.o Debug/stm32h7xx_hal_spdifrx.o Debug/stm32h7xx_hal_uart.o Debug/stm32h7xx_hal_uart_ex.o Debug/stm32h7xx_hal_pwr.o Debug/stm32h7xx_hal_pwr_ex.o Debug/stm32h7xx_hal_sram.o Debug/stm32h7xx_hal_flash.o Debug/stm32h7xx_hal_flash_ex.o Debug/stm32h7xx_hal_gpio.o Debug/stm32h7xx_hal_hash.o Debug/stm32h7xx_hal_hash_ex.o Debug/stm32h7xx_hal_pcd.o Debug/stm32h7xx_hal_pcd_ex.o Debug/stm32h7xx_ll_usb.o Debug/stm32h7xx_hal_hrtim.o Debug/stm32h7xx_hal_rcc.o Debug/stm32h7xx_hal_rcc_ex.o Debug/stm32h7xx_hal_crc.o Debug/stm32h7xx_hal_crc_ex.o Debug/stm32h7xx_hal_eth.o Debug/stm32h7xx_hal_tim.o Debug/stm32h7xx_hal_tim_ex.o Debug/stm32h7xx_hal_sai.o Debug/stm32h7xx_hal_sai_ex.o Debug/stm32h7xx_hal_sdram.o Debug/stm32h7xx_hal_qspi.o Debug/startup_stm32h753xx.o Debug/bsp_driver_sdram.o Debug/sdram_diskio.o Debug/fatfs.o Debug/diskio.o Debug/ff.o Debug/ff_gen_drv.o Debug/syscall.o -Wl,--end-group
    1>Debug/lcd.o: In function `initRA8877':
    1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(94): error : undefined reference to `lcdRegDataWriten'
    1>collect2.exe : error : ld returned 1 exit status
    1>make: *** [Debug/TH218_sln.elf] Error 1

    sorry for the delayed response

    waclawek.jan
    Super User
    September 19, 2018

    Post the sources, possibly reduced to a bare minimum which still compiles and produces the problem.

    JW

    T J
    T JAuthor
    Senior III
    September 19, 2018

    is this what you are after ?

    waclawek.jan
    Super User
    September 19, 2018

    Yes.

    And you have compiled and linked this and it still threw the above error?

    JW