Question
using the fsmc to boot from NOR and run with pSRAM -MCP - STM32F439
Posted on February 28, 2016 at 13:43
Hi.
I would like to understand wheather it is possible to use the FSMC of the STM32F439 to interface with a MCP module - NOR FLASH+pSRAM, where the address and data are shared and multiplexed . I see that there is a bank for NOR /PSRAM , but is it possible to work with both on the same chip ? will it be possible to boot from the nor and run with the RAM after ? does the driver support address/data multiplexing ? thank you ! Daniel