Skip to main content
swhite
Associate III
June 23, 2009
Question

Using/testing the PVD interrupt.

  • June 23, 2009
  • 2 replies
  • 588 views
Posted on June 23, 2009 at 21:33

Using/testing the PVD interrupt.

    This topic has been closed for replies.

    2 replies

    swhite
    swhiteAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:15

    Solved it :) The problem was another

    EXTI_DeInit();

    line in another part of the program. That was undoing the initialization for EXTI_Line16 :-Y

    swhite
    swhiteAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:15

    I'm having trouble using the PVD interrupt to do stuff at power-down. The

    interrupt doesn't seem to occur (can't debug during power-loss!) even when

    simulating it via software (calling PVD_Test()).

    Code:

    PVD_init(void)

    {

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);

    PWR_PVDLevelConfig(PWR_PVDLevel_2V9);

    PWR_PVDCmd(ENABLE);

    ...

    EXTI_DeInit();

    EXTI_StructInit(&exti_config);

    exti_config.EXTI_Line = EXTI_Line16;

    exti_config.EXTI_Mode = EXTI_Mode_Interrupt;

    exti_config.EXTI_Trigger = EXTI_Trigger_Rising;

    exti_config.EXTI_LineCmd = ENABLE;

    EXTI_Init(&exti_config);

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_InitStructure.NVIC_IRQChannel = PVD_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_Init(&NVIC_InitStructure);

    }

    PVD_IRQHandler(void)

    {

    ... Never get here!

    }

    PVD_Test()

    {

    EXTI_GenerateSWInterrupt(EXTI_Line16);

    }