Skip to main content
Associate
August 4, 2025
Solved

Using STM32H562ZI with I3C v1.0 compatible I3C Target endpoint

Hi,

I'm planning to use STM32H562ZI as I3C controller with an I3C v1.0 compatible Target endpoint. Since STM32 I3C IP supports I3C v1.1.1, will there be any potential issues on RSTDAA, ENTDAA, I3C Private Write, I3C Private Read or other electrical parameters with v1.0 ? Though I do not see any limitation based on v1.0 & v1.1.1 specifications (Apart from IBI mandatory byte and new CCCs), I'd like to hear from the community. Appreciate the help.

Thanks,
Srinath

This topic has been closed for replies.
srinathkpBest answer
Associate
August 10, 2025

ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.

This can be marked as resolved now.


2 replies

Billy OWEN
ST Employee
August 5, 2025

Hi @srinathkp 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

srinathkpAuthorBest answer
Associate
August 10, 2025

ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.

This can be marked as resolved now.