Skip to main content
This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
June 14, 2022

That link is to a minimalistic linux version which is to be run directly on the STM32F2xx.

> do I have to implement a full i2c slave that would emulate another discrete RTC?

Yes.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
June 14, 2022

That link is to a minimalistic linux version which is to be run directly on the STM32F2xx.

> do I have to implement a full i2c slave that would emulate another discrete RTC?

Yes.

JW

EMela
EMelaAuthor
Associate II
June 14, 2022

Thank you! I suspected that.

It would have been nice to use that instead of a discrete chip . But I assume it would be a lot of work to do a full implementation of a known device that works out of the box with a linux driver.