Question
Using Stm3240g firmware on the Stm32f4Discovery Board - Solved
Posted on April 17, 2012 at 10:55
I am working on Porting over the Stm3240g Board Firmware to the Stm32f4Discovery Board. The Boards both use the same chip stm32f407 - just different pinouts. Obviously there are compatibility issues on the Port connections.
* Currently I have BlinkLed working with PC.7 and PE.0 ports. * I have tried to Enable both of UART2 and UART4 with no success. * I have successfully connected it via USB as Mass Storage - Windows recognizes the USB Mass Storage - BUT it reports as 'Mass Storage fails to start'. I am using an SDCard connected - like the stm3240g board except that SD_DETECT is switched from PH13 to PH0. The System_stm324xx_eval.h has PLL_M=25 to PLL_M=8 for Clock which is needed for the USB connection. I do not know why the SDCard fails - the Card is tested as working. Anybody have any ideas ?