Skip to main content
gunccc
Associate II
Feb 6, 2023 8:54 AM UTC
Question

Using STM32 HRTIM to Transmit the Input Signal to the Output

0693W00000YA2qgQAD.pngHi,

I want to use STM32G474's HRTIM for my project.There is one input(A) and 2 output(B,C) signals.I need to check the input signals controls and then I want to transmit the 'A' signal as the output as the 'B' signal. It should be same as the A signal. I don't want to regenerate the output signal i want to transmit the A signal to the output as a B signal. This is my main purpouse. And for the C signal i need to reverse the A signal but again those all signals should have the same frequency. Is it possible to do it with HRTIM module?

This topic has been closed for replies.

1 reply

Associate
May 5, 2024 12:47 PM UTC

Hi!

I have the same problem, did you find the solution?