Skip to main content
RrW1
Associate III
Dec 1, 2020 11:16 PM UTC
Solved

Using STM32 FLASH memory

I am learning on using the STM32L431CC FLASH memory to store data after the microcontroller loses power. From compiling through Keil, I get:

Program Size: Code=34316 RO-data=1228 RW-data=364 ZI-data=1908

From the above, Is it correct that only 35Kbytes of FLASH are being used?

FLASH/ROM = Code + RO-data = 34316 + 1228 = 35544 bytes

Since the STM32L431CC uses Pages instead of Sectors for its FLASH, this is the code that I used to write into its FLASH memory:

HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR);
HAL_FLASHEx_Erase(&lFlashPage, &PageErrorStatus);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x0803F800, *pData1);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x0803F800 + 0x08, *pData2);
HAL_FLASH_Lock();

And the FLASH configuration that I used:

FLASH_EraseInitTypeDef lFlashPage;
lFlashPage.TypeErase = FLASH_TYPEERASE_PAGES;
lFlashPage.Banks = FLASH_BANK_1;
lFlashPage.Page = 127;
lFlashPage.NbPages = 1;

If the whole program only uses 35Kbytes of FLASH memory, does that also mean that the program only used FLASH Page 0 up to FLASH Page 17 (total of 36KBytes with 2KByte per page), and that it is safe to use FLASH page 127? The FLASH rewriting should not mess up the program itself would it? I should also note that I have not tried changing the Scatter File in Keil and don't know if I have to if the program won't touch Page 127 at all.

I also have a question regarding erasing the FLASH page. Would calling the function:

HAL_FLASHEx_Erase(&lFlashPage, &PageErrorStatus);

erase FLASH page 127 into all 0xFFFFFFFF? I did notice that at startup, if I did not write anything to FLASH, the data stored in the memory are 0xFFFFFFFF per block.

Any help would be appreciated. Thank you!

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
Dec 2, 2020 8:15 PM UTC

The RW-data section takes the space in both - RAM and FLASH - because it has to be initialized to non-zero values and those initialization values are stored in FLASH memory. Therefore:

FLASH/ROM = Code + RO-data + RW-data = 34316 + 1228 + 364 = 35908 bytes

> Why do people usually change the linker/scatter file when playing with the FLASH memory?

Because then compiler will show "code/data doesn't fit in FLASH memory" error in case the code+data reaches the forbidden addresses.

9 replies

DDong.2
Associate
Dec 2, 2020 2:21 AM UTC

​From the above, Is it correct that only 35Kbytes of FLASH are being used?

YES

​

 the program only used FLASH Page 0 up to FLASH Page 17 (total of 36KBytes with 2KByte per page), and that it is safe to use FLASH page 127? 

YES. The keil only flash your code to the flash. It didn't know if you use page 127​. Your code did it. Unless your code size extend to page 127 otherwise you can use page 127 as you want. You can notice all this flash memory is using start from 127. It makes sure the memeory will not mess with your code.

RrW1
RrW1Author
Associate III
Dec 2, 2020 5:55 AM UTC

Thanks for the answer! So, when is it required to change the Scatter file in Keil to allocate part of the FLASH for our own uses? Why do people usually change the linker/scatter file when playing with the FLASH memory?

DDong.2
Associate
Dec 2, 2020 7:32 AM UTC

I have no idea. I have never change the ​Scatter file.

Piranha
PiranhaBest answer
Principal III
Dec 2, 2020 8:15 PM UTC

The RW-data section takes the space in both - RAM and FLASH - because it has to be initialized to non-zero values and those initialization values are stored in FLASH memory. Therefore:

FLASH/ROM = Code + RO-data + RW-data = 34316 + 1228 + 364 = 35908 bytes

> Why do people usually change the linker/scatter file when playing with the FLASH memory?

Because then compiler will show "code/data doesn't fit in FLASH memory" error in case the code+data reaches the forbidden addresses.

RrW1
RrW1Author
Associate III
Dec 2, 2020 10:11 PM UTC

Thanks for clarifying that the FLASH/ROM takes Code + RO-data + RW-data.

In the example you gave, if the code/data exceeds the amount of FLASH available, wouldn't the program crash regardless of the changes made in the scatter file?

Piranha
Principal III
Dec 2, 2020 10:42 PM UTC

In your case you have 128 * 2 KB = 256 KB flash. If you reserve the last sector for user data section, then it is wise to reduce the available flash for compiler to 254 KB, because otherwise (someday) the compiler will happily fill the firmware code/data up to that last sector. It still doesn't exceed 256 KB and technically everything is fine, but the firmware now collides with your user data section.