Skip to main content
anas27
Associate
August 10, 2014
Question

Using ST-Link with STM32F439

Posted on August 10, 2014 at 20:58

Hi all,

I am planning on using the STM32F439 as I need as much performance as possible. As I understand it, to upload a program to the board I will need the ST-Link V2. Could someone please explain how I would connect the two together, i.e. which wire goes where?

Thanks for all the help.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    August 10, 2014
    Posted on August 10, 2014 at 23:41

    Just use a standard connector, and that way you can use regular pods/cables.

    http://infocenter.arm.com/help/topic/com.arm.doc.faqs/attached/13634/cortex_debug_connectors.pdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    anas27
    anas27Author
    Associate
    August 12, 2014
    Posted on August 12, 2014 at 08:26

    Thanks very much! Also, will online tutorials based on the discovery boards (with the debugger built in) be applicable to my setup? Sorry it's such a novice question!

    Tesla DeLorean
    Guru
    August 12, 2014
    Posted on August 12, 2014 at 14:12

    Applicability of code for other boards/designs will be dependent on how many differences there are in the designs, and the clock/pin/peripheral changes you will need to make to port the code to your board. The more similar the designs, the less work you'll have.

    You should spend a lot of time reviewing the schematics for as many reference designs using the STM32 parts as you can before designing/building your own. Read the data sheets and reference manuals until you are comfortable with the functionality and implementation.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    anas27
    anas27Author
    Associate
    August 16, 2014
    Posted on August 16, 2014 at 15:57

    Thanks a lot for the advice!