Skip to main content
dbmiller5
Visitor II
February 2, 2013
Question

Using ST Link on Discovery board as standalone ST Link

  • February 2, 2013
  • 2 replies
  • 863 views
Posted on February 02, 2013 at 09:12

I have

http://www.sainsmart.com/sainsmart-stm32f103rbt6-arm-cortex-m3-mini-development-board-code-jlink-v8-adapter.html

 (board only), and I need

JTAG debugger to program it.  Is it possible to use my F1 discovery as a JTAG debugger for the purpose of programming?  I am totally new to STM32, but I am excited to learn.  

Thanks, 

Dave
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    February 2, 2013
    Posted on February 02, 2013 at 11:15

    You should be able use a VL-Discovery to program it via the SWD connections. You'd need to remove the internal jumpered connections, and then wire up the SWDIO (JTMS), SWCLK (JTCK), and GND to the associated pins on the 20-pin JTAG header.

    In an ideal world you'd probably want NRST too.

    The SWD header does not provide for full JTAG functionality.
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    ken239955
    Associate II
    February 2, 2013
    Posted on February 02, 2013 at 21:24

    That is exactly how I am using my STM32F0DISCOVERY as clive describes it. You only need two wires plus ground.