RKore.1Associate IIIForum|Forum|4 years agoAugust 29, 2022QuestionUsing Nucleo 429ZI and implanting a simple SPI code , There are no signals on the SCK Mosi pins when sending data on SPI1Forum|Forum|4 years agoAugust 29, 20228 replies2317 viewsI am using SPI1 as a Master full duplex , and checking in the Nucleo 429 zi PA5 ------> SPI1_SCKThere is no clock , I using a scope and testing PA5 pin on the Nucleo 429 zi I attach the code , its very short code Here is the link to the pin description https://os.mbed.com/platforms/ST-Nucleo-F429ZI/testSPIsignals.7zSTM32F4 seriesSPI