Skip to main content
DSEO
Associate II
Feb 14, 2019 12:52 PM UTC
Solved

Using lcd_log.c library function

Hi!!

I'm using lcd_log.c to debug on the LCD.

LCD_UsrLog ("This is Line% d \ n", i);

Is there a way to change the starting position of text output?

It always starts at the same location and scrolls down.

Please, help me!!

    This topic has been closed for replies.
    AvaTar
    AvaTarBest answer
    Senior III
    Feb 14, 2019 1:16 PM UTC

    If you talk about the SPL code for a F3 (like the F3 discovery), review the line-related functions in source file stm32303c_eval_lcd.c in folder ...Utilities/STM32_EVAL/STM32303C_EVAL.

    3 replies

    AvaTar
    AvaTarBest answer
    Senior III
    Feb 14, 2019 1:16 PM UTC

    If you talk about the SPL code for a F3 (like the F3 discovery), review the line-related functions in source file stm32303c_eval_lcd.c in folder ...Utilities/STM32_EVAL/STM32303C_EVAL.

    DSEO
    DSEOAuthor
    Associate II
    Feb 15, 2019 6:02 AM UTC

    Oh I see!! thanks!!

    DSEO
    DSEOAuthor
    Associate II
    Feb 15, 2019 4:07 AM UTC

    No, I file use in Utilities\Log\lcd_log.c..

    file has 6 function below.

    void LCD_LOG_Init(void);

    void LCD_LOG_DeInit(void);

    void LCD_LOG_SetHeader(uint8_t *Title);

    void LCD_LOG_SetFooter(uint8_t *Status);

    void LCD_LOG_ClearTextZone(void);

    void LCD_LOG_UpdateDisplay (void);

    And I tested function like below.

    I want to change the location of the output text(This is Line..) , but I do not know where to fix it. (6 Function)

    void Log_demo(void)

    {

        uint8_t   i = 0;

        uint8_t   scroll_direction = 0;

        uint8_t   scroll_index = 0;

        /* Initialize LCD Log module */

        LCD_LOG_Init();

        /* Show Header and Footer texts */

        LCD_LOG_SetHeader((uint8_t *)"Test Debug LCD Monitor");

        LCD_LOG_SetFooter((uint8_t *)"");

        /* Output User logs */

        for (i = 0; i < 10; i++){

            LCD_UsrLog ("This is Line %d \n", i);

        }

    //    HAL_Delay(500);

        /* Clear Old logs */

        LCD_LOG_ClearTextZone();

        /* Output new user logs */

        for (i = 0; i < 30; i++) {

            LCD_UsrLog ("This is Line %d \n", i);

        }

        /* Check for joystick user input for scroll (back and forward) */

        while (1)

        {

            if (scroll_direction == 0)

            {

                LCD_LOG_ScrollBack();

                scroll_index++;

                if (scroll_index > 30)

                {

                    scroll_direction = 1;

                }

            }

            else

            {

                LCD_LOG_ScrollForward();

                scroll_index--;

                if (scroll_index == 0)

                {

                    scroll_direction = 0;

                }

            }

            HAL_Delay (10);

        }

    }