using Keil RL-RTX with STemWin
Dear Sir,
I'm using STM32F4-DISCOVERY. I've to run the STemWin on this board with keil RL-RTX. I've made all the necessary GUI and LCD configurations and have added GUI_X_RTX.c from the Segger folder in Keil uVision. I've packed the whole of the GUI part in a single task 'GRAPHICS' as follows in main function.
But my GRAPHICS task never runs.I'm not having any compiling or linking errors though.How can I use KEIL RL-RTX to do this job?I found examples of implementing emWin with embos ang freertos kernel, but haven't found any hint or anything to do it with Keil RL-RTX. I've done all my project with this. so can't just swich to some other RTOS. My main.c looks like this.
''''
#include <RTL.h>
#include ''stm32f4xx.h'' #include ''stm32f4_discovery.h'' #include ''GUI.h'' #include ''bsp.h''#include ''DIALOG.h''
OS_TID t_GRAPHICS;
OS_TID t_STEPPER;extern void MainTask(void);
extern void LED_Init (void); U16 COUNTER1;/*********************************************************************
* Externals *********************************************************************/ WM_HWIN CreateIntro(void); uint8_t GUI_Initialized = 0;* Main
*/ __task void GRAPHICS (void) {os_evt_wait_and(0x0002,0xffff); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);
//STM32f4_Discovery_LCD_Init();
/* Initilize the BSP layer */ BSP_Init();
/* Activate the use of memory device feature */ WM_SetCreateFlags(WM_CF_MEMDEV);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE);
/* Init the STemWin GUI Library */ GUI_Init();
/*WM_SelectWindow(WM_HBKWIN); WM_SetDesktopColor(GUI_BLACK);*/
GUI_Initialized = 1;
MainTask(); for (;;);
}__task void STEPPER (void) {
for(;;) {
os_evt_wait_and(0x0001,0xffff); /* my code*/}
}void BSP_Background (void)
{ static uint32_t LED_ticks = 0; static uint32_t POINTER_ticks = 0;if ( LED_ticks++ > 100 ) { LED_ticks = 0;
/* toggle LED1..4 each 100ms */ /* STM_EVAL_LEDToggle(LED4); STM_EVAL_LEDToggle(LED3); STM_EVAL_LEDToggle(LED5); STM_EVAL_LEDToggle(LED6);*/ }
if ( POINTER_ticks++ > 50 ) { POINTER_ticks = 0; /* Capture input event and updade cursor */ if(GUI_Initialized == 1) { BSP_Pointer_Update(); } }
}#ifdef USE_FULL_ASSERT
/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) *//* Infinite loop */ while (1) {}
} #endifvoid delay(__IO uint32_t nCount)
{ __IO uint32_t index = 0; for (index = (100000 * nCount); index != 0; index--); }__task void init (void) {
t_GRAPHICS= os_tsk_create(GRAPHICS,0); t_STEPPER= os_tsk_create(STEPPER,1); os_evt_set (0x0001, t_STEPPER); os_tsk_delete_self (); }
int main (void) {
LED_Init(); os_sys_init (init); /* Initialize RTX and start init */} ''''kindly someone help me to do this this....Just can't find what else I've to modify....