Skip to main content
Associate II
Nov 13, 2025 1:48 PM UTC
Question

Using external RAM with STM32U5G9-HSPI

Hi Everyone,

I am working on a project with TouchGFX. I'm working with STM32U5G9ZJT6 and I have an external RAM APS12808L-OBM-BA connected via HSPI (Fclk-hspi 100 MHz) in mapped mode.

 

The project is working, but the image animation are not working well. To solve it I have decided to increase the HSPI frecuency.

The APS12808L-OBM-BA memory can operate at up to 200MHz. However, when I exceed 118MHz, I can't map the memory. You can see a picture below reading the memory after mapping (you see "?").

Carlos_Aperton_0-1763041028096.png

I have changed the memory read latency (MR0 and MR4) to increase the Fmax.

I need all of suggestions for this issue.

Thanks in advance all

 

Carlos_Aperton_1-1763041362659.png

Carlos_Aperton_2-1763041490365.png

Carlos_Aperton_3-1763041569967.png

 

 

 

 

5 replies

Andrew Neil
Super User
Nov 13, 2025 2:21 PM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

In particular, please give details of your hardware - could there be a hardware issue with speeds >118 MHz ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Nov 19, 2025 5:58 AM UTC

Hi Andrew,

I have kept the same track length (about 18.5mm) and close to the microcontroller.

Carlos_Aperton_0-1763370932803.png

 

Andrew Neil
Super User
Nov 19, 2025 10:12 AM UTC

Please also show the schematic.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
May 13, 2026 9:08 AM UTC

Any news?