Skip to main content
KEria.1
Associate II
Jun 17, 2021 4:02 PM UTC
Solved

Using DMA with UART on STM32H753ZI and getting HAL_DMA_ERROR_TE (Transmission Error)

Hello,

I am trying to set the UART5 TX with the DMA. I am using Cube, and in the GUI I selected UART5 to asynchronous, and added DMA for UART5_TX. Then, in the generated code, I added this part as I didn't see initialization for the DMA (inside the MX_DMA_Init()):

 /* Peripheral DMA init*/
 hdma_uart5_tx.Instance = DMA1_Stream0;
 //hdma_uart5_tx.Init.Channel = DMA_CHANNEL_4;
 hdma_uart5_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_uart5_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_uart5_tx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_uart5_tx.Init.PeriphDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_uart5_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_uart5_tx.Init.Mode = DMA_NORMAL;
 hdma_uart5_tx.Init.Priority = DMA_PRIORITY_MEDIUM;
 hdma_uart5_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 HAL_DMA_Init(&hdma_uart5_tx);
 
 __HAL_LINKDMA(&huart5,hdmatx,hdma_uart5_tx);

The Main function, I didn't do much except I added this code in the while(1):

while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
	 if (HAL_UART_Transmit_DMA(&huart5,au8ch, 1) == HAL_OK)
	 {
		 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_SET);
	 }
	 else
	 {
		 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_RESET);
	 }
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */

Which is a code to transmit the first byte of an array. I connected the Nucleo-H753ZI board pins to a terminal software, and I didn't get anything. (Note that I was able to get something without using the DMA). The LED turned ON, which means the function is returning HAL_OK, but still nothing on the screen.

I tried to debug the code, I put a breakpoint in the function "void HAL_DMA_IRQHandler(DMA_HandleTypeDef *hdma)" and it stops there, which means it got the interrupt to send something, but then it goes into this autogenerated code:

if(IS_DMA_STREAM_INSTANCE(hdma->Instance) != 0U) /* DMA1 or DMA2 instance */
 {
 /* Transfer Error Interrupt management ***************************************/
 if ((tmpisr_dma & (DMA_FLAG_TEIF0_4 << (hdma->StreamIndex & 0x1FU))) != 0U)
 {
 if(__HAL_DMA_GET_IT_SOURCE(hdma, DMA_IT_TE) != 0U)
 {
 /* Disable the transfer error interrupt */
 ((DMA_Stream_TypeDef *)hdma->Instance)->CR &= ~(DMA_IT_TE);
 
 /* Clear the transfer error flag */
 regs_dma->IFCR = DMA_FLAG_TEIF0_4 << (hdma->StreamIndex & 0x1FU);
 
 /* Update error code */
 hdma->ErrorCode |= HAL_DMA_ERROR_TE;
 }
 }
...
...
...
/* manage error case */
 if(hdma->ErrorCode != HAL_DMA_ERROR_NONE)
 {
 if((hdma->ErrorCode & HAL_DMA_ERROR_TE) != 0U)
 {
 hdma->State = HAL_DMA_STATE_ABORT;
 
 /* Disable the stream */
 __HAL_DMA_DISABLE(hdma);
 
 do
 {
 if (++count > timeout)
 {
 break;
 }
 }
 while((((DMA_Stream_TypeDef *)hdma->Instance)->CR & DMA_SxCR_EN) != 0U);
 
 /* Process Unlocked */
 __HAL_UNLOCK(hdma);
 
 if((((DMA_Stream_TypeDef *)hdma->Instance)->CR & DMA_SxCR_EN) != 0U)
 {
 /* Change the DMA state to error if DMA disable fails */
 hdma->State = HAL_DMA_STATE_ERROR;
 }
 else
 {
 /* Change the DMA state to Ready if DMA disable success */
 hdma->State = HAL_DMA_STATE_READY;
 }
 }
 
 if(hdma->XferErrorCallback != NULL)
 {
 /* Transfer error callback */
 hdma->XferErrorCallback(hdma);
 }
 }
 }

Any idea what I may be missing?

This topic has been closed for replies.
KEria.1
KEria.1Best answer
Associate II
Jun 17, 2021 9:18 PM UTC

@Community member​  and @TDK​ Thank you both for your help.

I figured it out. I had to build void HAL_UART_TxHalfCpltCallback(UART_HandleTypeDef *huart) function in which I put the values I need to send, also in the Cube GUI, I had to make it Normal not circular in order to send the data only once.

It is working to send one array now. Thanks!

Karim

12 replies

TDK
Jun 17, 2021 4:19 PM UTC

Make sure the au8ch buffer is somewhere accessible by DMA. What memory address is it at?

"If you feel a post has answered your question, please click ""Accept as Solution""."
KEria.1
KEria.1Author
Associate II
Jun 17, 2021 4:22 PM UTC

0x2001fff4

I initialized it at the beginning of the main()

TDK
Jun 17, 2021 4:26 PM UTC
That address is in DTCM, which is not accessible to DMA.
https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices
"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
Jun 17, 2021 4:42 PM UTC

Have you read the article I gave link to? Read it. Reread it. For gcc (which is the default compiler for CubeIDE), you have to read the section about the linker script.

JW

KEria.1
KEria.1Author
Associate II
Jun 17, 2021 5:15 PM UTC

Thanks, I read it, and reread it, and re-reread it.. Here is what I did:

in the file: STM32H753ZITX_RAM.ld I changed this code (I put what I changed in the comments below in the file) as recommended in solutions 1 and 2.

I only deployed solution 1 at first and it didn't fix it, so I added this section at the end.

 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 } >RAM_D1 AT> FLASH /* was >RAM AT> RAM_EXEC*/
 
 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss secion */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)
 
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM_D1 AT> FLASH /* was >RAM*/
 
 /* User_heap_stack section, used to check that there is enough RAM left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM_D1 AT> FLASH /* was >RAM*/
 
/* I also added this part: */
 .dma_buffer : 
 {
 *(.dma_buffer)
 } >RAM_D2

Then I added the code in the main.c in the previous comment.

#if defined( __ICCARM__ )
 #define DMA_BUFFER \
 _Pragma("location=\".dma_buffer\"")
#else
 #define DMA_BUFFER \
 __attribute__((section(".dma_buffer")))
#endif
 
DMA_BUFFER unsigned char au8ch[4] = {70,54,35,4};

But still, I got nothing. Any advice?

waclawek.jan
Super User
Jun 17, 2021 6:33 PM UTC

> But still, I got nothing.

That's an equivalent of "it does not work" and is not helpful.

So, how are your variables allocated now? What's in the mapfile? How is RAM_D2 set? Do you change the linker script you are actually using?

I don't use Cube/CubeIDE/Eclipse so can't really help in this detail.

JW

KEria.1
KEria.1Author
Associate II
Jun 17, 2021 7:22 PM UTC

Does that answer your question?

/* Specify the memory areas */
MEMORY
{
 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
 RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
 RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
 RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
 ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}

KEria.1
KEria.1Author
Associate II
Jun 17, 2021 7:50 PM UTC

New update, so the previous memory map I did in the RAM.ld, I did the same in flash.ld file, and it started to transmit data now.

However, for some reason it is not transmitting what I am sending, and it is continuously transmitting. (not stopping after the 4 bytes I am sending)

KEria.1
KEria.1AuthorBest answer
Associate II
Jun 17, 2021 9:18 PM UTC

@Community member​  and @TDK​ Thank you both for your help.

I figured it out. I had to build void HAL_UART_TxHalfCpltCallback(UART_HandleTypeDef *huart) function in which I put the values I need to send, also in the Cube GUI, I had to make it Normal not circular in order to send the data only once.

It is working to send one array now. Thanks!

Karim