Skip to main content
kahseng05
Associate II
March 18, 2015
Question

Using ch2 and ch4 as input capture

  • March 18, 2015
  • 26 replies
  • 4730 views
Posted on March 18, 2015 at 13:44

Hello,

I'd like to use channel 2 and channel 4 of TIM2 as input capture. Channel 2 work fine, but channel seems returning the timer counter. Here's the code:

GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_ICInitTypeDef TIM_ICInitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM16, ENABLE);
/*Trigger pin configuration*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_1);
TIM_TimeBaseStructure.TIM_Prescaler = 71;
TIM_TimeBaseStructure.TIM_Period = 60000;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM16, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OC1Init(TIM16, &TIM_OCInitStructure);
TIM_CtrlPWMOutputs(TIM16, ENABLE);
TIM_Cmd(TIM16, ENABLE);
TIM_SetCompare1(TIM16, 10);
/*Echo Pin configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOD, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_2);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_PWMIConfig(TIM2, &TIM_ICInitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11,GPIO_AF_1);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_4;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_PWMIConfig(TIM2, &TIM_ICInitStructure);
TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset);
TIM_SelectMasterSlaveMode(TIM2,TIM_MasterSlaveMode_Enable);
TIM_Cmd(TIM2, ENABLE);

#clive1
    This topic has been closed for replies.

    26 replies

    Tesla DeLorean
    Guru
    March 28, 2015
    Posted on March 28, 2015 at 14:46

    What part are we talking about in this thread? The STM32F3?

    I wouldn't do the division at that point a) it loses all the precision you have, and b) interferes with the numbers wrapping in the 32-bit space during the subtraction.

    This would measure the periodicity between two edges, either rising, falling, or both, depending on how you configured the timer. To measure frequency and duty you'd need to be observing both edges. and making three consecutive measurements.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    kahseng05
    kahseng05Author
    Associate II
    March 28, 2015
    Posted on March 28, 2015 at 15:03

    Ya, it is STM32F3. May you show me where should I do the division?

    Measurement at the rising edge, falling edge?

    Tesla DeLorean
    Guru
    March 28, 2015
    Posted on March 28, 2015 at 15:28

    With integer math you'd usually want to do any division last, so as to maintain precision, as you're about to throw away the fractional portion.

    cc[0] = TIM_GetCapture2(TIM2);
    delta[0] = (cc[0] - cc[1]) / 72; // time between two measurements in microseconds, from 72 MHz clock
    cc[1] = cc[0];

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    March 28, 2015
    Posted on March 28, 2015 at 15:38

    With rounding

    delta[0] = ((cc[0] - cc[1]) + 36) / 72;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    kahseng05
    kahseng05Author
    Associate II
    March 28, 2015
    Posted on March 28, 2015 at 16:32

    Thanks clive. You said that I have to measure 3 consecutive values to get duty and frequency. The timer interrupt is executed every time the timer overflow as the period is set to 0xFFFFFFFF. so how can I observe both edges and make 3 measurements.

    Tesla DeLorean
    Guru
    March 28, 2015
    Posted on March 28, 2015 at 23:58

    Sounds like you've got the wrong interrupt enabled. I'd really like not to have to code your project for you.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..