Skip to main content
PZarc
Associate
March 23, 2020
Question

Using Array to toggle outputs

  • March 23, 2020
  • 3 replies
  • 1106 views

Hi,

I want to try use an array to set particulars outputs, base on values in that arrays

I have initiated two dimensional array like in example below:

uint8_t obrPr[4][4] = {

 {0,0,1,1},

 {1,1,0,0},

 {0,1,1,0},

 {1,0,0,1}

  };

This is sequences, when the output should be ON and when OFF.

Using simple for loop, tried to toggle the outputs, but it does not working for me, like below:

if (Joystick[1] >= 2100) { 
 
		 for(z=0,x=0; z < 64000; z++,x++){} // this is just for check whether the for loop is working
 
		 for(i=0; i<4; i++){
			 for(j=0; j<4; j++){
 
		 HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, obrPr[0][j]); //IN1
	 HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, obrPr[1][j]); //IN2
	 HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, obrPr[2][j]); 	 //IN3
	 HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, obrPr[3][j]); //IN4
		 	 }
		 }
 	 }

I'm using interrupts of TIM3 to fire the outputs with different frequencies and this above code is inside the PeriodelapsedCallback{} of TIM3.

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
 
if(htim->Instance == TIM3) {
...
}

Those frequencies are changing in main loop by joystick and I use below example code for it:

if (((Joystick[1] >= 2160) && (Joystick[1] <= 2650)) && tPr[0] == 1 ) {
 
		TIM3->CNT = 0; // Set Tim3 cnt as 0
 	HAL_TIM_Base_Start(&htim3); // Enable Tim3
 		HAL_TIM_Base_Start_IT(&htim3); // enable interrupts for Tim3
 
 		TIM3->ARR = 65000;
	 	tPr[0] = 0, tPr[1] = 1, tPr[2] = 1, tPr[3] = 1, tPr[4] = 1;
 
 } else if (btnState == 1 && licznik_TIM3 == 1) {
	} else if (((Joystick[1] >= 2703) && (Joystick[1] <= 3107)) && tPr[1] == 1 ) {
 
	 TIM3->CNT = 0;
	 HAL_TIM_Base_Start(&htim3);
	 	HAL_TIM_Base_Start_IT(&htim3);
		TIM3->ARR = 1600;
	 tPr[0] = 1, tPr[1] = 0, tPr[2] = 1, tPr[3] = 1, tPr[4] = 1;
} else if (((Joystick[1] >= 2086) && (Joystick[1] <= 2099)) && tPr[4] == 1) {
 
	 	HAL_TIM_Base_Stop(&htim3);
	 	HAL_TIM_Base_Stop_IT(&htim3);
	 	TIM3->CNT = 0;
	 	IN1_OFF;
	 	IN2_OFF;
	 	IN3_OFF;
	 	IN4_OFF;
	 	TIM3->ARR = 400;
	 tPr[0] = 1, tPr[1] = 1, tPr[2] = 1, tPr[3] = 1, tPr[4] = 0;
}

This above part is working correctly, but not in case, when the array is use. Using array, it seems the for loop stop on the last 4 step and only GRN & BLUE leds are lighting all the time, when the joy is moved to his right side. Looking at the values in obrPr array, the last step is 1,0,01, what fire the PD12 and PD15 output (32F411EDISCOVERY with STM32F407VGTx)

obrPr[4][4] = {

 {0,0,1,1},

 {1,1,0,0},

 {0,1,1,0},

 {1,0,0,1}

  };

The below code, which I would like to exchange with the array, to shrink the amount of lines of the code is working OK. Means the led are switching as expected:

//Definitions at the beginning
#define IN1_ON HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, GPIO_PIN_SET)
#define IN1_OFF HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, GPIO_PIN_RESET)
#define IN2_ON HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, GPIO_PIN_SET)
#define IN2_OFF HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, GPIO_PIN_RESET)
#define IN3_ON HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, GPIO_PIN_SET)
#define IN3_OFF HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, GPIO_PIN_RESET)
#define IN4_ON HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, GPIO_PIN_SET)
#define IN4_OFF HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, GPIO_PIN_RESET)
 
...
	
 if (Joystick[1] <= 1918) {
 
	 if (sekw == 1) //PD 12
	 {
		 IN2_OFF; //LED_ORANGE_PD13
		 IN4_OFF; //LED_BLUE_PD15
		 IN1_ON; //LED_GREEN_PD12
	 	 IN4_ON; //LED_BLUE_PD15
	 	 }
	 else if (sekw == 2) //PD 14
	 	 {
		 IN4_OFF; //LED_BLUE_PD15
	 	 IN3_ON; //LED_RED_PD14
	 	 }
	 else if (sekw == 3) //PD 13
	 {
		 IN1_OFF; //LED_GREEN_PD12
	 	 IN2_ON; //LED_ORANGE_PD13
	 	 IN3_ON; //LED_RED_PD14
	 	 }
	 else if (sekw == 4) //PD 15
	 {
		 IN3_OFF; //LED_RED_PD14
	 	 IN4_ON; //LED_BLUE_PD15
	 	 }
	 	 ++sekw;
	 if (sekw == 5)
	 {
	 sekw = 1;
	 }
	 	 }

I would like to ask for help and explain, why is not working.

Regards

Piotr,

This topic has been closed for replies.

3 replies

TDK
March 23, 2020
		 for(i=0; i<4; i++){
			 for(j=0; j<4; j++){
 
		 HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, obrPr[0][j]); //IN1
	 HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, obrPr[1][j]); //IN2
	 HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, obrPr[2][j]); 	 //IN3
	 HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, obrPr[3][j]); //IN4
		 	 }
		 }

What is i doing here? Why is j looping at all? Why is everything inconsistently indented?

Code seems to be doing exactly what you're asking it to do, which is basically the following:

		 HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, obrPr[0][3]); //IN1
	 HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, obrPr[1][3]); //IN2
	 HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, obrPr[2][3]); 	 //IN3
	 HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, obrPr[3][3]); //IN4

"If you feel a post has answered your question, please click ""Accept as Solution""."
PZarc
PZarcAuthor
Associate
March 23, 2020

TDK,

Thanks for update

for(i=0; i<4; i++){
 for(j=0; j<4; j++){
 
 HAL_GPIO_WritePin(LED_GREEN_PD12_GPIO_Port, LED_GREEN_PD12_Pin, obrPr[0][j]); //IN1
 HAL_GPIO_WritePin(LED_ORANGE_PD13_GPIO_Port, LED_ORANGE_PD13_Pin, obrPr[1][j]); //IN2
 HAL_GPIO_WritePin(LED_RED_PD14_GPIO_Port, LED_RED_PD14_Pin, obrPr[2][j]); 	 //IN3
 HAL_GPIO_WritePin(LED_BLUE_PD15_GPIO_Port, LED_BLUE_PD15_Pin, obrPr[3][j]); //IN4
 }
 }

Hope now is better.

So, why j is looping? Because I'm using it to red the values in columns and this way set 1 or 0 in the parameter for HAL_GPIO_WritePin. Each column include info whether the particular of the 4 pins should be on(1) or off(0) in one time.

Suppose the loop is going to i = 4 & j = 4 and then leaves this loop. As the first parameter if (Joystick[1] >= 2100) is still met, again jumping to to the for loop and repeat it n times, till the condition of the if (Joystick[1] >= 2100) is true.

Is not that?

In debug mode, jumping line by line, the pins are toggled correctly.

PZarc
PZarcAuthor
Associate
March 25, 2020

Ok, I found the reason

Thanks