Skip to main content
ayaka
Associate II
Jul 8, 2010 11:47 PM UTC
Question

using ADC to convert two channels

Posted on July 09, 2010 at 01:47

using ADC to convert two channels

    This topic has been closed for replies.

    3 replies

    swhite2
    Associate II
    May 17, 2011 11:58 AM UTC
    Posted on May 17, 2011 at 13:58

    I guess I don't understand your reluctance to use DMA. It is very easy to configure and you can still use interrupts so you know when the results are updated.

    There is only one ADC  conversion result register so unless you're careful the last value can be easily overwritten.

    t1_it
    Visitor II
    May 17, 2011 11:58 AM UTC
    Posted on May 17, 2011 at 13:58

    If the issue is that there is insufficent time to read the ADC data register before it is overwritten by the next conversion, then I would have thought that you could increase the sampling times for the two channels to give you a longer time to grab the data.

    picguy2
    Associate III
    May 17, 2011 11:58 AM UTC
    Posted on May 17, 2011 at 13:58

    You can use injected channel for up to 4 ADC conversions without DMA.  Look at ST’s  injected channel code.  The first channel converted result ends up in ADC_JDR4, the second in ADC_JDR3.

    With DMA you can start a continuous conversion with ADC values going to  RAM.  No interrupts required.  Simply grab the latest value from RAM.  I have used this with one DMA channel.  I think it might work with two or more.