Skip to main content
Gpeti
Senior
October 7, 2019
Question

Use STM32H7 ETM without debugging tool

  • October 7, 2019
  • 24 replies
  • 7199 views

I need to use the ETM on a STM32H753 but without debugging tool. The idea is to record the execution trace all the time, and when the firmware encounter a critiical issue, output the trace to an external tool or program it to flash for later analysis. It is designed to work in operational mode, not through a debugging tool.

The documentation of ARM is very confusing on the topic. Some documents mentions the ETB (Embedded Trace Buffer) other documents mentions the ETF (Embedded Trace FIFO) but I couldn't really understand which is doing what.

I don't really understand what functionality of the STM32 to use to implement what I need, and also how to do it. Strangely enough, I didn't find any code example of discussion about this online. it's surprising because recording execution trace sounds like a very interesting functionality in safety critical environments in particular.

This topic has been closed for replies.

24 replies

Tesla DeLorean
Guru
October 7, 2019

Tends to be the domain of debugger writers, ARM should have app notes, but presupposes familiarity with HW/SW at this level.

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0242b/DDI0242.pdf

Others on the forum have built trace HW, so might have some specific insight.

@Bob Boys​ any thoughts on the internal mechanics ARM can share?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gpeti
GpetiAuthor
Senior
October 7, 2019

Thank you Clive. So I've read again the related section in the ref Manual. What I deduced is that ARM provides several ways to store the execution trace and among them ST chose to implement the ETF.

This ETF can be setup in Circular Mode, which looks like the mode I need:

"3. Circular buffer mode

The trace memory is used as a circular buffer. Trace data is captured into the Trace

memory starting from the location pointed to by the write pointer register. Even when

the trace memory is full, incoming trace data continues to be overwritten into the trace

memory until a stop condition occurs.

In this mode, the ETF stores the trace data on-chip, so the trace log size is limited to

that of the ETF SRAM, 4 Kbytes in this case. Being a circular buffer, if the FIFO

becomes full, incoming trace data overwrites the oldest stored data and the oldest

stored data is lost. Therefore the contents of the trace buffer represent the most recent

activity of the processor, up to the point when the buffer was stopped, rather than all

the activity since the trace was started.

There are three possible methods to read out the buffer contents once the trace stops:

– via the Trace port - with the TPIU enabled, the contents of the buffer are output

over the Trace port. This can be done by setting the DRAINBUF bit in the

ETF_FFCR register.

– via the Debug port - the debugger can read the buffer via the RRD register that is

accessible over the system APB-D.

– by software - the processor can read the buffer via the RRD register, since the

APB-D is accessible from the system bus."

The reference manual also gives the description of the ETF registers. I will try to implement the functionality based on this but I find the documentation ia bit "light" to do so without wasting days. So I would still appreciate tips, code examples or application notes.

Tesla DeLorean
Guru
October 7, 2019

Like I said, I think ARM has app notes it shares with debugger developers. You might find reference to them via open source debugger projects, things like Open OCD spring to mind. ARM's forums may be a better place to ask, and might have debugger specific sub-forums.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gpeti
GpetiAuthor
Senior
October 8, 2019

So I've based my implementation on two documents, the section on ETF in STMicro STM32 reference manual and ARM's Trace Memory Controller Reference Manual. In the latter in particular there is a sequence to setup the ETF:

Circular Buffer mode

The recommended standard usage model in this mode is as follows:

1. Wait until TMCReady is equal to one.

2. Program the MODE Register for Circular Buffer mode.

3. Program the FFCR Register. ARM recommends that you set the TrigOnTrigIn,

FOnTrigEvt, StopOnFl, EnTI, and EnFt bits. This enables formatting, inserting a trigger

when a trigger is observed on TRIGIN, and following a delay corresponding to the value

of the TRG Register, flushing and then stopping the TMC.

4. Program the TRG Register, to control the amount of buffer to be dedicated to the period

after a trigger is observed.

5. Set the TraceCaptEn bit in the CTL Register. This starts the trace session.

6. Wait until TMCReady is equal to one. This indicates that the trace session is over.

7. Read the contents of the trace buffer by performing successive reads to the RRD Register,

until the value 0xFFFFFFFF is returned.

8. Clear the TraceCaptEn bit in the CTL Register.

The notion of triggers is more or less incomprehensible so I've stupidly written the registers as described without really understanding what's going on.

But actually I can't go very far in my debug: it looks like the ETF registers are not accessible (they're all read to 0 either through the debugger or through my embedded software). There is probably an "enable" bit somewhere to activate or clock the TMC or ETM or ETF or who knows what macrocell.

Here is the piece of quick and dirty code I tried, every register is read to 0 and not modified by this code

HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART3_UART_Init();
 
// enable ETM trace
*ETM_PRGCTRL = 1;
 
// enable ETF circular mode
*ETF_FFCR = 0x00001123; // ARM recommends to set bits TRIGONTRIGIN FONTRIGEVT STOPONFL ENTI AND ENFT
*ETF_TRG = 16; // number of 32 words to capture
*ETF_CTL = 1; // enable trace
 
i = 1000;
while(i--)
 asm("nop"); // ******** processing just to fill the trace
 
while ( ((*ETF_STS) & (1<<2)) == 0 );
 
printf("*ETF_RRD=0x%x\r\n", *ETF_RRD);
printf("*ETF_RRD=0x%x\r\n", *ETF_RRD);
printf("*ETF_RRD=0x%x\r\n", *ETF_RRD);
printf("*ETF_RRD=0x%x\r\n", *ETF_RRD);
 
*ETF_CTL = 0; // disable trace

Tesla DeLorean
Guru
October 8, 2019

I'd expect you'd need to unlock each unit via it's LAR (Lock Access Register) on CM7 chips.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gpeti
GpetiAuthor
Senior
October 8, 2019

Indeed ! There is an ETM_LAR and an ETF_LAR, i've just found it. So now I can write in ETM registers but not in ETF :(

To be continued :)

Gpeti
GpetiAuthor
Senior
October 9, 2019

I've found this comment on the Segger forum:

"(...) unfortunately ST made the decision with the STM32H7 to "hide" some trace related modules behind the APB instead of AHB as it is usual for Cortex-M7. That way the generic trace init process becomes highly ungeneric."

ST people, could you comment on that ?

Tesla DeLorean
Guru
October 9, 2019

The multicore nature of the H7 was not disclosed​ for many years, this adds to the complexity significantly and explains some of the awkwardness in the design/structure. I suspect ARM and ST experimented with some things.

​

I wouldn't expect ST engineers familar with internals at this level to wade into open forum discussions.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gpeti
GpetiAuthor
Senior
October 9, 2019

"I wouldn't expect ST engineers familar with internals at this level to wade into open forum discussions." I can understand that. But on the other hand I'm just trying to use a functionality that they sell on their product.

Gpeti
GpetiAuthor
Senior
October 9, 2019

In which way is the H7 multicore ?

Tesla DeLorean
Guru
October 14, 2019

It has always been a multi-core design, it goes a long way to explaining why it is otherwise significantly more complex/convoluted in design compared to the F7, and why most of the resources are a bus ride away from where you would normally put them. It uses a SWD protocol capable of talking to multiple access ports.

0690X00000AqLXZQA3.jpg

0690X00000AqLXkQAN.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Gpeti
GpetiAuthor
Senior
October 9, 2019

An interesting point to note: the ID registers of ETM can be read properly from the debugger (even without unlocking ETM_LAR). The ID registers of ETF are read to 0...

Gpeti
GpetiAuthor
Senior
October 9, 2019

Great ! Just noticed that the STM32H7 ref manual is inconsistent on debug mappings !

0690X00000ApMFUQA3.jpg

0690X00000ApMIJQA3.jpg

Gpeti
GpetiAuthor
Senior
October 9, 2019

So if I use the address 0x5C014000 I can at least read/write ETF registers properly.

Pavel A.
October 14, 2019

If you're familiar with Python, this project can be useful: https://github.com/cortexm/pyswd

-- pa

Bob Boys
Visitor II
October 14, 2019

Hello

Sorry to take so long to reply to this - it was Arm TechCon show time last week.

The best way to do this is to access the circular RAM and read it with your software.

This way you do not need external hardware to read the 4 bit + clk signals of the TracePort output.

This method has the advantage to track the instructions no matter how fast your CPU is running.

There are CoreSight registers you need to configure to get trace data stored in this buffer.

I believe the trace data is comprised of the program flow changes, not each individual instruction executred. You, like the debbugger, must reconstruct the executed instruction details. The timestamps are not output with every instruction - I am not sure of the rule used here.

A good way to see how the ETM trace works is to use Keil uVision (free eval version will work) and a ULINKpro (US$ 1,250).

Good luck !

Bob Boys

Arm

*******************************************************************

 See RM0433 (Rev6), page 3104:

 https://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/c9/a3/76/fa/55/46/45/fa/DM00314099/files/DM00314099.pdf/jcr:content/translations/en.DM00314099.pdf

Circular buffer mode

The trace memory is used as a circular buffer. Trace data is captured into the Trace

memory starting from the location pointed to by the write pointer register. Even when

the trace memory is full, incoming trace data continues to be overwritten into the trace

memory until a stop condition occurs.

In this mode, the ETF stores the trace data on-chip, so the trace log size is limited to

that of the ETF SRAM, 4 Kbytes in this case. Being a circular buffer, if the FIFO

becomes full, incoming trace data overwrites the oldest stored data and the oldest

stored data is lost. Therefore the contents of the trace buffer represent the most recent

activity of the processor, up to the point when the buffer was stopped, rather than all

the activity since the trace was started.

There are three possible methods to read out the buffer contents once the trace stops:

– via the Trace port - with the TPIU enabled, the contents of the buffer are output

over the Trace port. This can be done by setting the DRAINBUF bit in the

ETF_FFCR register.

– via the Debug port - the debugger can read the buffer via the RRD register that is

accessible over the system APB-D.

– by software - the processor can read the buffer via the RRD register, since the

APB-D is accessible from the system bus.

Gpeti
GpetiAuthor
Senior
October 15, 2019

Thank you for your answer. I don't understand how buying a $1000 device will help me to understand how the ETF/DWT/ETM registers need to be programmed, as their programming by the ULINKPRo and Keil will be hidden and anyway different than what I need to do (since ULINK uses the Trace pins).

Here is the status of my work on the topic.

I configure the ETF as follows:

*ETF_LAR = 0xC5ACCE55;
 *ETF_FFCR = 0x00001123; // ARM recommends to set bits TRIGONTRIGIN FONTRIGEVT STOPONFL ENTI AND ENFT
 *ETF_TRG = 16; // number of 32 words to capture
 *ETF_CTL = 1; // enable trace

Then the ETM:

*ETM_LAR = 0xC5ACCE55;
 *ETM_CONFIG = (*ETM_CONFIG) | 0x00031F30;
 *ETM_PRGCTRL = 1;

What is missing is (from what I've been told by a specialist in ARM architectures) to setup the DWT to trigger the trace. This is where it is still confusing as no ARM documents explain clearly the link between DWT and ETM. I understood that DWT uses signals CMPMATCH[N] to signal a match to the ETM (??).

I tried to setup DWT comparator 0 to accept all flash memory accesses like that:

*DWT_COMP0 = 0x08000000; // start fo flash address
 *DWT_MASK0 = 24; // ignore 24 least significant bits
 *DWT_FUNCT0 = 0x00000008; // b1000	ETM trigger on PC match

It's not working : the bit READY of EFT_STS remains at 0 and the bit EMPTY of same register remains at 1.

However the bit MATCH of DWT_FUNCTION0 is set, meaning that the comparator has matched once

I really feel like I'm playing riddles...

Cheers

Bob Boys
Visitor II
October 17, 2019

Hello

If you have a ULINKpro (or Segger J-Trace or IAR iJetTrace) you can observe a working ETM system to save time. You can examine various registers to see what works.

ULINKpro can also access ETB - although I have not tried it on your processor.

Bob Boys

Arm

Gpeti
GpetiAuthor
Senior
October 18, 2019

I don't have a trace capable device (yet). It sounds surprising that it is the only solution to understand how this is working...