Skip to main content
zsong.2
Visitor II
August 10, 2022
Question

use one GPIO to do Duplex communication

  • August 10, 2022
  • 2 replies
  • 654 views

hi ,

I have to STM32 chip, how to use one GPIO to do Duplex communication bettween this two STM32 ?

thanks

    This topic has been closed for replies.

    2 replies

    S.Ma
    Principal
    August 10, 2022

    No details will yield fuzzy answers.

    There is a protocol for 1 wire interface, like the ones to communicate with smart batteries, which could be worth exploring.

    Otherwise, open drain usart on tx pin with external pull up and sw swap rx tx to get bidirectional. You will need to implement protocol and collisions.

    Piranha
    Principal III
    August 10, 2022

    A push-pull with an internal pull-up and a series 1k resistor for safety performs much better. And with a SWAP configuration bit the same half-duplex communication can be done on Rx pin.