Use one DMA channel with 2 different IPs ?
Hello.
The project I am actually working on uses several peripherals such as USART ADC SPI etc.
I am trying to use as much DMA as I can, but there is something that I miss in the reference manual and on the internet.
Can I use ONE channel with TWO streams of TWO independant IPs ?
Can I use ONE channel with TWO streams of ONE IP ?
For instance with a STM32F427:
UART4 uses dma1 stream2 with channel4 and dma1 stream4 with channel 4
and
USART2 uses dma1 stream6 with channel4 and dma1 stream0 with channel 4
In this example :
Could I use the two streams for UART4 or only one stream at a time ?
Could I use every streams that I quoted for UART4 and USART2 (D1S2C4, D1S4C4, D1S6C4 and D1S0C4) at the same time ?
Thank you,
Have a nice day.