Skip to main content
lars-kristian
Associate II
June 8, 2009
Question

Use of the StdPeriph_Lib 3.0 with Keil Compiler

  • June 8, 2009
  • 4 replies
  • 849 views
Posted on June 08, 2009 at 13:15

Use of the StdPeriph_Lib 3.0 with Keil Compiler

    This topic has been closed for replies.

    4 replies

    lars-kristian
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:14

    Hi ,

    I'm trying to get the new StdPeriph_Lib V3.0 work with the Keil uVision3 Environment. It seems like these two don't work togehter properly. I did a couple of tries in the last days but I had no success with it. I always get some errors and warnings about undefined functions (standard ADC and DMA functions).

    The main problem is, that I have to use the different Interrupthandlers of the 3 ADCs. Keil only supports one Interrupt Handler (ADC_IRQHandler) and not the two of the new FW (ADC1_2_IRQHandler & ADC3_IRQHandler).

    Is there a chance to successfully migrate from the FW 2 to the StdPeriph_Lib 3 in the Keil Environment?

    Regards,

    Lars

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:14

    Quote:

    I have to adjust it to my requirements.

    Yes, of course you do! 8-)

    lars-kristian
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:14

    Hi,

    I'll try to explain it in a different way. The standard startup file (vector table) of the Keil compiler doesn't include these functions. So I have to include them by myself. I just compared the Keil and the ST startup files and

    saw that they're different in the names of the interrupt functions.

    Now it is clear, that I have to adjust it to my requirements.

    Regards,

    Lars

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:14

    Quote:

    Keil only supports one Interrupt Handler (ADC_IRQHandler) and not the two of the new FW (ADC1_2_IRQHandler & ADC3_IRQHandler).

    What do you mean by that?? :-?

    Keil does not place any restrictions at all on this - you can load whatever functions you like into the vector table to handle the interrupts!