Question
Use I2S_CKIN external clock source for SPI?
Posted on April 04, 2018 at 17:08
Is it possible to use the I2S_CKIN external clock source for SPI rather than come off the peripheral clock? From the reference manual it appears that this external clock is available as a source only when the SPI is in 'I2S Mode'. Is there a workaround? I am using an STM32F765. Thanks!
#i2s_ckin #spi