Skip to main content
Associate II
May 2, 2025 5:24 PM UTC
Solved

USBx MSC demo not working on stm32h5 discovery board

I've just brought the stm32h573i-dk dev board and what to become familiar with Threadx and USBx. I have a uni project coming up that I would like to use the board as a msc device but struggling to get the board to enumerate with the PC. I have tried to get majority of the USBx reference designs up and running. They compile fine but nothing happens when I connect the board to a PC on cn17 ( the non stl-link usb). Is there anything I'm doing  wrong to get it up and running . Is there something I need to enable to for the USB port to work? 

 

I also have a couple of u5 and h5 nucleo boards I would also like to get up and running With various forms of USB Once I have the discovery board working. Any pointers would be greatly welcome. Thanks

SidewinderBest answer
Associate II
May 12, 2025 9:50 PM UTC

Hi FBL,

I have just revisited looking at the USBx examples but used a different USBc cable and  all examples

work. It looks like a power only cable had got mixed in with the cables.

3 replies

ST Technical Moderator
May 5, 2025 9:38 AM UTC

Hi @Sidewinder 

Did you insert SD card before application is started?

Would you specify boards revision. Is it MB1677-C01?
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
SidewinderAuthorBest answer
Associate II
May 12, 2025 9:50 PM UTC

Hi FBL,

I have just revisited looking at the USBx examples but used a different USBc cable and  all examples

work. It looks like a power only cable had got mixed in with the cables.

Associate
Dec 8, 2025 6:10 PM UTC

I’m having the same issue. The STM32H573I-DK example USBPD_SRC_UX_Host_MSC compiles normally, but when I plug a USB flash drive into the board, nothing happens. The board doesn’t detect or respond to the device.