Solved
USB virtual com port can't receive data when device reboot
Hello,
I experienced a phenomenon in which the USB port was not reconnected.
This phenomenon occurs when a USB port is connected to the product and reboots.
I check my device manager.
When i turn off product, com port also disappear.
and product reboot then com port appear.
But i can't receive any data.
When i reconnect USB cable then communication work well.
Summary
- USB virtual com port can't receive data when device reboot.
- In the same state as above, USB cable reconnect then USB connect well.
I need your support.
Thanks. best regards.