Skip to main content
JWink.1
Associate
May 27, 2023
Question

USB stopped connecting to STM32F405.

  • May 27, 2023
  • 3 replies
  • 2635 views

I have an Adafruit STM32F405 Feather Express. I am compiling / uploading with Arduino IDE V2.1.0 with Windows 11 64. The board worked well for about a week, but no longer connects/shows up as Port 5 of USB. I was successfully connecting and uploading code with the Arduino IDE. After a few days away from the project, I discovered my STM32F405 Express no longer connects to the USB. I did attempt to install MS WDAC - see below.

When I jump B0 to +3.3 and press reset, (I hear a USB connect sound) under "Universal Serial Bus devices", "STM BOOTLOADER" appears in the device manager; it's always visible w/ or w/o the 405 if "View -> Show hidden devices" is checked). Unplugging the USB after a BO+reset generates a "disconnect" sound. Nothing appears under "Ports (COM & LPT)". When it was working, I could see it under "Port 5". Now, neither the STM32, nor any other device, is visible on the IDE under "Tools -> Port".

With the device manager and looking the STM BOOTLOADER Device Manager properties / Events tab / "Device install requested", I see "Device USB\VID_0483&PID_DF11\2065326F4D31 requires further installation." A B0+reset generates a "connect" sound, but no sound is generated otherwise.

The code I previously uploaded which simply sets up two PWM channels appears to be working - I can see waveforms on the 6 and 9.

If I connect a Nano to the USB, "USB-SERIAL CH340 (COM6)" appears and the Arduino IDE sees it as "COM6".

After seeing a caution icon on the "Windows Security - Actions recommended" icon in the task bar, I did attempt, apparently unsuccessfully, to install the Microsoft Windows Defender Application Control about the time the problem occurred. MS WDAC.

I did uninstall/reinstall Arduino IDE 2.1.0 The problem still exists. Same content in the Device Manager. Uninstalled/reinstalled "STM32 MCU based boards by STMMicroelectronics" 2.5.0 Per the instructions on Arduino IDE Setup setup page, "STM32 Cores by STMicroelectronics" no longer appears to exist, used a new version.

Any suggestions or hints would be appreciated.

Thanks -Jim

Edit: Adding the Event Viewer log

=============================================================

Installation configuration

Level: Information

time stamp: 5/27/2023 13:03:45

=============================================================

Device USB\VID_0483&PID_DF11\2065326F4D31 was configured.

Driver Name: oem180.inf

Class Guid: {88bae032-5a81-49f0-bc3d-a4ff138216d6}

Driver Date: 05/07/2018

Driver Version: 1.1.0.0

Driver Provider: STMicroelectronics

Driver Section: USB_Install

Driver Rank: 0xFF0001

Matching Device Id: USB\VID_0483&PID_DF11

Outranked Drivers:

Device Updated: false

Parent Device: USB\VID_045B&PID_0209\6&38487f98&0&1

=============================================================

Level: Error.

Time stamp: 5/27/2023 13:03:45

Device USB\VID_0483&PID_DF11\2065326F4D31 had a problem starting.

=============================================================

Driver Name: oem180.inf

Class Guid: {88bae032-5a81-49f0-bc3d-a4ff138216d6}

Service: WinUSB

Lower Filters:

Upper Filters:

Problem: 0x0

Problem Status: 0xC00000E5

    This topic has been closed for replies.

    3 replies

    JWink.1
    JWink.1Author
    Associate
    June 8, 2023

    Got it working! I deleted C:\Users\...\AppData\Local\Arduino15\packages\stm32duino and C:\Users\...\AppData\Local\Arduino15\packages\STMicroelectronics then reloaded.

    Tesla DeLorean
    Guru
    June 9, 2023

    Could STM32 Cube Programmer not see/use the "STM32 BOOTLOADER" device?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    JWink.1
    JWink.1Author
    Associate
    June 9, 2023

    Attempting to install Microsoft's Vulnerable Driver Blocklist was the only thing I think might have done it. It was working fine, I took a break for a few days. During that break, I installed. A few days later, I tried to connect and it no longer worked.