Skip to main content
Associate
Oct 2, 2026 3:34 AM UTC
Question

USB pins PA11, PA12 failing short during hot plugin of type C port (STM32H563VG)

Hi ST Team,

In our design, the USB pin pairs from PA11, PA12 our failing short multiple times during hot plug in of type C port to power the board. The USB pin pairs does not directly go to type C port rather it goes through this chip PCMF3USB3S (ESD + EMI filter) from Nexperia. Currently we do not have any ESD protection on VBUS pin. The VBUS +5V currently generates 3.3VDD to power the STM32H56V3G on our board. There is also a diode as connected reverse b/w VBUS +5V and 3.3Vdd output as recommended in AN4899.

Can you please give us some insights on why this could be happening and what would be the possible solution

 

 

1 reply

ST Technical Moderator
Nov 2, 2026 8:33 AM UTC

Hi ​@Roy_B1027 

Repeated damage to PA11/PA12 during hot plug could be caused by ESD or voltage transient. Check the USB protection orientation, placement, and ground connection, and consider whether VBUS and the 3.3 V rail need additional transient protection.

The image doesn’t show enough of the circuit to confirm the cause. Compare with the reference board design provided.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL