Skip to main content
Senior
Mar 18, 2026 11:16 AM UTC
Solved

USB-PD: STM32G0 with only one CC line configuration question

This is looking for more info from this original post

* https://community.st.com/t5/stm32-mcus-embedded-software/i-am-using-usb-pd-system-with-stm32g071rb76-processor-there-are/m-p/219760#M53483

 

 

With a stm32 chip with only one CC line could i connect both of the CC lines together.

  • This is a DFP
  • I don't need VCON support

If i were to do this could i still figure out what the orientation is?  

Brenden_PLUSBest answer
Senior
Mar 18, 2026 1:13 PM UTC

Well you can also talk over USB PD.  So in theory if there was a message that sent back orientation then this could be solved.  But i guess since the UFP is always connected to CC1,  then there's no way to get the orientation because the host doesn't know what orientation it is.

 

So i guess this is a dumb question.  

2 replies

TDK
Mar 18, 2026 12:56 PM UTC

The primary purpose of the CCx pins is to detect orientation. If you tie them together, you will not be able to detect orientation and some USBPD features may not work.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Brenden_PLUSAuthorBest answer
Senior
Mar 18, 2026 1:13 PM UTC

Well you can also talk over USB PD.  So in theory if there was a message that sent back orientation then this could be solved.  But i guess since the UFP is always connected to CC1,  then there's no way to get the orientation because the host doesn't know what orientation it is.

 

So i guess this is a dumb question.