Skip to main content
Remo Steiger
Visitor II
Oct 21, 2017 12:56 PM UTC
Question

USB OTG with STM32CubeF4

Posted on October 21, 2017 at 14:56

Hi all

I am using the STM32F429ZE microcontroller with STM32CubeF4 (V1.16.0) library.

For my next project I need to switch between USB device and host mode. (Depends if a host/device is connected.)

The hardware has an USB OTG full-speed interface and was used successfully for other projects with USB device or USB host functionalities.

I didn't found any dual role example in the STM32_USB_Device_Library and STM32_USB_Host_Library included in STM32Cube. However the STM32_USB-Host-Device_Lib (V2.2.0) seems to support this feature but uses the standard peripheral library.

Do the USB libraries in STM32Cube support the OTG feature and if so, how can I switch between host and device mode?

If STM32Cube does not support OTG functions, do I have to convert the STM32_USB-Host-Device_Lib from standard peripheral library to the HAL library or is there any other solution?

Thank you very much for your efforts!

Remo
    This topic has been closed for replies.