For sure, you don't need the ID pin connected since you don't use OTG mode. :) Bad news: For the VBUS pin, I think you have to connect it to the USB connector/adapter... in all cases. :( I hope this helps you.
i want to use my STM32F107VC as a peripheral with virtual COM-port. Do i have to connect the VBUS- and ID-pin to the USB-connector? I need these two pins for other purposes. Thanks, C.H.
The Vbus connection to PA9 is needed for two reasons:
1. HW detecting that host is connected and the USB voltage is valid 2. used as a reference for connecting internal 1k5 pull-up between D+ and Vbus to signal, that the device is full-speed and ready for enumeration. All info can be found in RefMan (RM0008).