Skip to main content
Pilot B
Associate III
Apr 2, 2018 9:30 PM UTC
Question

''USB On-The-Go Host'' or ''USB Host''?

Posted on April 02, 2018 at 23:30

Hi everyone,

I'm working on a board based on STM32F4XX. We plan to support USB Host on it for communication(CDC). I found there are 'USB On-The-Go Host' and 'USB Host' libraries. I'm not sure which one to use.

First, I downloaded examples from STM32CubeF4: 

http://www.st.com/en/embedded-software/stm32cubef4.html

  

and found 'STM32Cube_FW_F2_V1.7.0\Middlewares\ST\STM32_USB_Host_Library' V3.2.2. That is the 'USB Host' library.

Later, I also found 'USB on-the-go Host and device library (UM1021)'

http://www.st.com/en/embedded-software/stsw-stm32046.html

This is 'USB On-The-Go Host' library V2.2.0. I found this is very different from the above 'USB Host' Library such as architectures, files and folder structures. For example, this is from usb_conf.h of the sample project:

/****************** USB OTG MODE CONFIGURATION ********************************/

#define USE_HOST_MODE

//#define USE_DEVICE_MODE

//#define USE_OTG_MODE

Interestingly, there is another product in our company that supports 'USB Device'. That product used the 'USB On-The-Go Device' library. So it has this in the usb_conf.h:

/****************** USB OTG MODE CONFIGURATION ********************************/

//#define USE_HOST_MODE

#define USE_DEVICE_MODE

//#define USE_OTG_MODE

As the engineer who worked on that product no longer works for the company any more, I don't know why he used 

'USB On-The-Go Device' library instead of the 'USB Device' library. 

So my questions:

1. Should I use 'USB On-The-Go Host' or 'USB Host' library? Or either one will work?

2. If I'd like to have an eval board to try this USB Host, what is the cheapest board I should use? For example, will this '

STMicroelectronics P-NUCLEO-USB002

' work?

https://www.digikey.ca/products/en/development-boards-kits-programmers/evaluation-and-demonstration-boards-and-kits/787?k=nucleo%2064

 

Thanks everyone!

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    Apr 2, 2018 10:04 PM UTC
    Posted on April 03, 2018 at 00:04

    For a user facing USB-FS port the STM32F4-DISC1 has a Micro-AB on the south end.

    https://www.mouser.com/new/stmicroelectronics/stm32f4discovery/

     

    https://www.mouser.com/ProductDetail/STMicroelectronics/STM32F407G-DISC1

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Pilot B
    Pilot BAuthor
    Associate III
    Apr 3, 2018 12:42 AM UTC
    Posted on April 03, 2018 at 00:42

    Hi Clive One,

    Thank you so much for your reply.

    For the first question, do you know if I should use 

    'USB On-The-Go Host' or 'USB Host' library?

    Thanks again!

    Tesla DeLorean
    Guru
    Apr 3, 2018 3:02 AM UTC
    Posted on April 03, 2018 at 03:02

    I'm on the peripheral/mass-storage side of the fence, USB host drivers not really my thing, I don't have a useful opinion here.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Pilot B
    Pilot BAuthor
    Associate III
    Apr 4, 2018 3:44 PM UTC
    Posted on April 04, 2018 at 17:44

    Hello everyone,

    I'd like to second this question.

    Basically, if I need to implement USB Host, should I use the 'USB On-The-Go Host'(UM1021) library or 'USB Host' library(UM1720)?

    Thanks!

    waclawek.jan
    Super User
    Apr 4, 2018 7:53 PM UTC
    Posted on April 04, 2018 at 19:53

    UM1021 is SPL-based, UM1720 is Cube-based.

    SPL is an older 'library', Cube is newer.

    (We ought to have a FAQ for this somewhere, btw.)

    JW

    Pilot B
    Pilot BAuthor
    Associate III
    Apr 4, 2018 10:23 PM UTC
    Posted on April 04, 2018 at 22:23

    Hi waclawek.jan,

    Thank you so much for your reply. 

    So I guess both libraries will work. But which one is better? Or are they equally good?

    Thanks again!